Szukaj często zadawanych pytań
Are spacers available for the leveling feet of NetShelter cabinets?
Issue:
It may be difficult to level a row of cabinets using the leveling feet only due to height differences in the concrete pad.
Product Line:
NetShelter SX, SV
Environment:
All versions and serial ranges.
Cause:
Cabinet rows need to be leveled.
Resolution:
Please use AR7605 spacer kit. Each kit includes 160 pieces: (120 x 8mm) and (40 x 2.25mm)
It may be difficult to level a row of cabinets using the leveling feet only due to height differences in the concrete pad.
Product Line:
NetShelter SX, SV
Environment:
All versions and serial ranges.
Cause:
Cabinet rows need to be leveled.
Resolution:
Please use AR7605 spacer kit. Each kit includes 160 pieces: (120 x 8mm) and (40 x 2.25mm)
Opublikowano dla:APC Poland
Dowiedz się więcej
Dowiedz się więcej