Szukaj często zadawanych pytań
Is there tech support or drivers available for APC-4902, USB1284 or 19008?
Issue:
Technical support is required.
Product Line:
Cables and Connectivity Solutions
Environment:
USB to Parallel, USB Extension, USB to IEEE1284
Cause:
Need drivers or other technical support.
Resolution:
The APC-4902, USB1284 and 19008 are all 'plug-n-play.' They do not require drivers.
For technical support on APC-4092, USB1284 or 19008 please contact APC Cables.
Phone: 888-370-6688 in North America
email: support@apccables.com
Opublikowano dla:APC Poland
Dowiedz się więcej
Dowiedz się więcej