Szukaj często zadawanych pytań
ISX-PDU; How to wire and configure the user input and output contacts via the User Connection plate
Issue:
How to wire and configure the user input and output contacts via the PDU User Connection plate
Product line:
ISX-PDU
Environment:
All models, all serial numbers
Cause:
User Connections to the PDU Monitoring Unit (Brains) is done thru the User Connection plate. User connections may be for EPO interface, input and output contacts.
Resolution:
Please refer to attached PDF files detailing the User Connection plate and how to configure the PDU user input and output contacts via the PDU PowerView display contacts screen.
Opublikowano dla:APC Poland
Załączniki
Dowiedz się więcej
Dowiedz się więcej