Szukaj często zadawanych pytań
Symmetra PX 250/500: What happens when EPO is activated?
Issue:
Symmetra PX 250/500; What does the EPO (Emergency Power Off) trip
Product line:
Symmetra PX 250/500
Environment:
All serial numbers
Cause:
What occurs when the EPO on a Symmetra PX 250/500 button is engaged?
Resolution:
When the EPO is activated, UPS output breaker Q2 and the battery breakers are tripped. The Power Modules (inverter), and if in Static Bypass operation, the UPS will turn off.
Opublikowano dla:APC Poland
Dowiedz się więcej
Range:
Dowiedz się więcej
Range: