Szukaj często zadawanych pytań
Are APC Cat 6 Patch Panels color coded for 568B or 568A?
Issue:
The installer needs to know the color code on the rear of the Cat 6 patch panel.
The installer needs to know the color code on the rear of the Cat 6 patch panel.
Product Line:
Cables and Connectivity Solutions, Patch Panels
Cables and Connectivity Solutions, Patch Panels
Environment:
CAT6PNL-24, CAT6PNL-48
CAT6PNL-24, CAT6PNL-48
Cause:
Installers need to know if the patch panel has the color code they require.
Installers need to know if the patch panel has the color code they require.
Resolution :
The CAT6PNL-xx series of Patch Panels have both 568B and 568A color codes. Opublikowano dla:APC Poland
Dowiedz się więcej
Dowiedz się więcej