Szukaj często zadawanych pytań
Why does ISX Manager/StruxureWare Central display the incorrect Kilowatt value when utilizing the Physical Layout or ISX Operations feature for my Metered/Switched Rack PDU product?
Issue
Incorrect Kilowatt (kW) values are being reported within ISX Manager or ISX/StruxureWare Operations tools from my Metered or Switched Rack PDU.
Product Lines
- ISX Manager
- ISX Central
- ISX Operations
- StruxureWare Data Center Operations
- AP78XX and AP88XX Metered Rack PDUs
- AP84XX Metered By Outlet Rack PDUs
- AP79XX, AP89XX, and AP86XX Metered Rack PDUs
- ISX Manager Physical Layout Tool - All Versions
- ISX or StruxureWare Operations - All Versions
- All serial numbers
Cause
APC has identified a problem that causes the Physical Layout or StruxureWare Central Operations to display the incorrect Kilowatt (kW) value. The Metered (AP78XX) and Switched (AP79XX) Rack PDU's as well as Inline Current Meters (AP7155, AP7175) that have 3.X.X firmware report their voltage and load to the ISX Manager or StruxureWare Central via SNMP, which displays the kW value through the Physical Layout or StruxureWare Operations tool. The problem that occurs stems from the Metered/or Switched Rack PDU and inline current meters reporting incorrect voltage. PDUs that operate on voltages, such as 208, 230, and 240 volts, will actually report 120 volts. This causes the kW value to appear "half" of its true value.
Resolution
With rpdu revision 3.7.4 and higher, these values can now be changed via the web UI on your device. Alternatively, these values can be changed via SNMP on most prior rpdu APP revisions. If you are experiencing this issue and need help fixing these values, please contact APC for assistance.