Browse FAQs



APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units . APC Unit Identification ... FM Air/ Water /Glycol W= Water Cooled F= Water Cooled D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled ... W= Hot Water ... Humidifier D= Downflow ... coil C= Chilled Water ... Humidifier D= Downflow C= Chilled Water ... Main C= Chilled Water W= Water Cooled ... G= Glycol Cooled BA=208 ... ... Humidifier D= Downflow W= Water Cooled ... G= Glycol Cooled D= Downflow W= Water Cooled
How does a chilled water actuator work on an acrc301h to control dew point after a power loss?
Upon restart, the fans start first to allow the sensors some time to recognize the air temperature and humidity as well as the fluid ...
Why do I need refrigerant traps in my piping?
All Air Cooled Cooling Units ... Data Center Cooling ... Oil is easily trapped in a discharge muffler, so it should be placed in the horizontal or downflow portion of the piping, as close to the compressor as possible. ... A: Whenever a condenser is located above the compressor, an inverted trap or check valve should be installed at the condenser inlet to prevent liquid refrigerant from flowing backwards into the compressor during off cycles.
What are the operational conditions for an InRoom (Stulz) Unit
... (Stulz) Unit . ... precision air conditioning units operate within the ... Chilled water -/ cooling water pipes: Maximum water head pressure: ... ... piping between the cooling unit and the air ... ... condenser and the cooling unit : 5 m ... is below the cooling unit Entering water temperature (EWT ... Leaving water temperature (LWT) for CW coil: 12°C (53.6°F) ... Cooling fluid (DX): 30% Glycol ... Chilled water medium (CW): 0% Glycol ... Downflow units with an external static pressure: 20 Pa (0.08 in w g)
InRow RC Standard and Optional Features
Data Center Cooling ... 1-The Standard Features of the InRow Rc Coolling Unit are as follow: Variable Speed Fans ... Chilled Water Flow Meter ... Data Partion Trough (Allows removal of RC unit without disrupting cabling)
Video: How to set up load assist on a Uniflair unit.
... on a Uniflair unit . ... Gen 1 and Chilled Water Units . Uniflair units with push button ... and all Uniflair Chilled Water Units . ... up a Uniflair unit to turn on ... ... to make the unit come on as ... ... two or more units and they must ... Press the ARROW unit you get to Sleep Mode Settings. ... (This is the temp you want the unit to turn on and help) ... Then press ENTER to go to Fan Cyclical Start. ... (This allows the fans to run to keep the air moving after temp or humidity has activated load assist)
ACSC1XX Spare Parts List
This document contains the Spare Parts List for ACSC1XX units . ... Please contact Cooling Tech Support to confirm the part numbers before quoting as some may have changed. ... CONDENSATE PUMP WIRE ASSY CP JUMPER (for activation without the water sensor kit) ... Condenser Fan 200mm Mixed Flow (INDIVIDUAL FAN ) ... EVAPORATOR FAN MODULE ASSY - 17 KW IR ... FAN 12VDC 60x25mm 25CFM ROHS (individual fan ) ... FAN FUSE NTC COMPLETE 818 PCB CRAC
Will the EcoAisle replace the tradition HACS offering
... to data center cooling with it's EcoAisle ... This flexible system adapts to both hot and cold aisles to address the wide range of data center cooling challenges faced by today's IT and facilities managers. When used with room, row, or external cooling systems the flexible aisle containment will maximize cooling system efficiencies by eliminating mixing and balancing airflow to enable increased operating temperatures and reduce fan energy. For facilities leveraging air or water economizers this systems is adaptable to maximize free cooling hours.
Inrow Chilled Water Units Internal Volumes
Issue: Inrow Chilled Water Units Internal Volumes
What is the Difference between Glycol and Chilled water?
Product line: All Water Cooled and Chilled Water Units .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.