Browse FAQs



What is the maximum number of XR frames allowed with a Symmetra PX 20, 40 and 80kw solution?
Symmetra PX; What ... maximum number of XR frames allowed with a Symmetra PX solution? Symmetra PX 20, ... ... maximum number of XR frames allowed with a Symmetra PX solution is 4 . ... size of the Symmetra PX Main Frame ... For a Symmetra PX 20 or ... number permitted is 4 fully populated (Battery Frames ) XR frames . ... a runtime of 1 hr 40 mins ... ... of addresses for XR frames . ... a fully populated XR frame is SYCFXR8 ... ... consists of the XR frame with 8 ... There are 4 Battery Units in ... this equals an XR frame with 32 ...
E3 error message on the Symmetra Extended Run Battery Frame (XR frame)
The XR frame of a single phase Symmetra displays E3 ... mainframe indicates an XR Frame Fault. Symmetra Power Array Symmetra RM Symmetra LX ... message on the Symmetra XR Frame is an ... communication between the Symmetra mainframe and the Symmetra Extended Run ( XR ) Battery Frame ... ... between the two frames where the Power ... located in the XR Frame. ... function of the UPS if it were ... ... that event the UPS goes on battery ... ... card on the Symmetra Extended Run Frame ... 1 ) Disconnect the ... back of the Symmetra Extended Run Battery ...
Single Phase Symmetra XR Frame Compatibility
Issue Single Phase Symmetra XR frames are compatible only with certain UPS systems.
Symmetra PX1-PX2; What happens when PX1, PX2 and 250/500k PX is EPO'd
Symmetra PX ... describes how the Symmetra PX reacts to ... ... , from a single point by activating ... ... circuit in the Symmetra PX is activated ... or in the XR Frame (80kw ... ... tripped on ISX PDU . There is no power on the output of the XR Battery Frames or on the output of the Symmetra PX UPS . ... Only the Battery CBs on XR frames will be tripped. Customer would need to have optional shut trip on Upstream CB to turn off input power to UPS . ... All Battery CBs on battery frames and Q2 will be tripped ... Reset EPO switch and follow proper procedures to restart UPS
Mounting the Symmetra LX in a 2 post rack
Symmetra LX ships with a 4 post rail kit ... safely mount the UPS system and any associated XR frames in a 2 post rack.
Symmetra Power Array reads "Bypass Out of Range"
Symmetra Power Array shows ... Symmetra Power Array ... This document describes one of the reasons ... a North American Symmetra Power Array may ... ... operation of a Symmetra Power Array, ... ... default, the Symmetra Power Array comes ... ... input of the Symmetra to a 240vac ... ... " of the Symmetra Main Intelligence Module ... ... (0's or 1's ). ... indicates whether the Symmetra's Input Voltage Jumper ... ... equal to " 1 ", then ... ... refer to chapter 4 in their Symmetra User's Manual. ... procedure, the UPS MUST be fully ... 1 . Turn the ... ... rear of the Symmetra . ... front of the Symmetra .
How to change the Input Voltage Select Jumper on a Symmetra Power Array
... environment of my Symmetra Power Array and ... Symmetra Power Array Before the UPS is started up ... : UPS must be completely ... 1 . Switch the ... 2. Open the input circuit breaker located on the front of the UPS . 3. Open and lockout the circuit breaker for the circuit that feeds the UPS . 4 . Remove all battery modules from the UPS . 5. Disconnect any extended run ( XR ) battery frames from the UPS . ... 1 . Refer to figure below. ... 3. Replace the voltage select access panel and continue with connecting the UPS to utility power.
Video: PDU Outlet Panel Replacement on Symmetra LX & Symmetra RM UPS Systems
1 ) Remove the screws in the four corners of the existing PDU panel or blanking plate.
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... operation while the PDU , UPS , or XR Battery Cabinet is ... 1 . Never work ... ... electricity to the PDU , UPS , or XR Battery Cabinet, ... 4 . Wear appropriate ... ... working on the PDU , UPS , or XR Battery Cabinet. ... from the equipment frames PSX/ PDU side panel installation ... a PSX or PDU . ... next to a PDU or UPS , then a PSX/ PDU side panel ( ... installed on the PDU or UPS . ... A PSX/ PDU side panel kit ... ... new PSX/ PDU side panel. 1 . Remove the ...
Batteries discharged to a low voltage in a single phase Symmetra frame
Single phase Symmetra battery modules are ... Symmetra Power Array Symmetra RM Symmetra LX 1 .) If ... ... to place the UPS into a bypass ... ... installed in a Symmetra frame, it ... If the Symmetra is powered down ... ... to place the UPS into a bypass ... All Symmetra and Symmetra RM units ship ... : Symmetra LX was designed ... ... only applies to Symmetra Power Array and Symmetra RM. The Symmetra will not be ... ... modules in connected XR frames ). Once the system has fully charged the one fresh battery installed in the UPS , the discharged batteries can be installed in the system one at a time to be recharged.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.