Browse FAQs



Where can I get support for APC and MGE Products?
Power Generation Systems Power Ready Notebook Cases
Configuring Microsoft Vista, Windows 7, 8, & 10, Windows 2008 & 2012 to safely shutdown without using APC's PowerChute software.
Once this happens, you can set up a desktop or server's power options in the same way as a laptop .
Steps to take when moving a Symmetra Power Array from one location to another
... receive your Symmetra Power Array, it ... "Unpacking and Installing Frame) to ... least temporarily in case you need to ... back to the APC or if you ...
What are some issues I may encounter when using an APC Back-UPS with a generator?
... stays on battery power while attached to ... ... to on battery power : All APC Back-UPS ... All APC Back-UPS ... ... stays on battery power while attached to ... ... to on battery power : SOLUTION: APC recommends that Back ... In most cases , to desensitize ... will need to install the Powerchute software ... ... Powerchute software is installed , you can ... Note about Building-size generators - Generally, generators used to back up an entire building or facility, such as those used for hospitals, are sized large enough and are of good enough quality that any APC UPS will operate fine.
Video: How do I create a direct connection between a computer and a APC networked enabled product?
... computer and a APC networked enabled product ... Rack Power Distribution Products ( ... Laptop or computer with ... ... (depends on APC /Schneider Electric ... Connect the crossover (or straight through, in the case of gigabit) cable. ... After completing the above configuration, for our example, we are having the APC device look at the computer as its default gateway and having the computer look at the APC device as its default gateway. ... From the computer, you should now be able to ping the IP of the NMC, in our case 192.168.1.2.
Will opening the case of my Smart-UPS or Back-UPS product void my warranty?
Will opening the case of my Smart-UPS or Back-UPS product void my warranty? ... Opening the enclosure of your Smart-UPS or Back-UPS products will void ... Do not open the case of your UPS. Please contact APC Support if you need assistance with your UPS or Warranty service ... These can be safely installed by an end user, but the UPS must be fully de-energized. (Turned off, unplugged from utility power , batteries disconnected.)
Why does my AP7867 Blade Server PDU go straight to overload when first powered on?
My AP7867 Rack PDU reports an overload immediately after power has been applied to it. ... In some cases , the embedded Network Management Card may not have been reset to defaults during final testing. ... In this case , please follow the steps below in order to clear the overload. ... Use the default " apc " for both unless you have changed these settings. ... The overload condition should clear and the PDU should be ready for user. Please contact APC Technical Support if you still experience an overload problem.
Computer will not automatically reboot after UPS has shutdown and restarted
All APC UPS ... a problem with APC UPS's or with ... ... circumstances - with APC or any other ... ... enter when the power supply senses input power when plugged into ... ... ON: When power is cycled on ... ... OFF: When power is cycled on ... ... STATE: When power is cycled on ... Off when the power was lost. In many cases , the computer ... using the system setup menu which can ... If this parameter is set to Always Off then an APC UPS cannot reboot ... on when the power is cycled independent of ... the PC prior to power being turned off.
Equipment connected to a Back-UPS product turns off unexpectedly and/or reboots.
All APC Back-UPS ... ... Follow the input power cord of the ... ... product provide backup power in the case of a power disturbance. ... not require backup power should be plugged ... ... event of a power problem. ... in the event power failed for an ... ... equipment in the case of a power disturbance. APC NEVER RECOMMENDS BATTERY ... ... , try to power the unit up ... ... in, contact APC at Technical Support ... ... its available battery power ... only supply battery power for a limited ... In some cases , depending on ... minutes of battery power .
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... describes how to install an acdc1010 Hot ... Install , A Rack ... ... when removing/ installing side panels from ... APC does not recommend ... ... is receiving input power , observe the ... ... Cabinet, in case of an emergency ... ... required to correctly install your Rack Expansion ... ... existing system, install two 21 U ... -mm) enclosure . ... page 5 before installing any side panels ... ... you plan to install a Rack Expansion ... ) must be installed on the PDU ... available from APC . Attach the ... ... 1070-mm enclosures ... -mm) enclosures :


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.