Consulter notre FAQ
{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}
Can the NetShelter AV busbar be installed into other NetShelter cabinets?
Issue:
AR8395 mounts to the accessory rail in the cabinet so it should be able to install into any NetShelter cabinet.
Product Line:
AR8395
Environment:
All versions and serial ranges.
Cause:
AR8395 description says that it's for the NetShelter AV cabinets.
Resolution:
The AR8395 can be installed into any NetShelter cabinet that has 20U vertical mounting space available.
AR8395 mounts to the accessory rail in the cabinet so it should be able to install into any NetShelter cabinet.
Product Line:
AR8395
Environment:
All versions and serial ranges.
Cause:
AR8395 description says that it's for the NetShelter AV cabinets.
Resolution:
The AR8395 can be installed into any NetShelter cabinet that has 20U vertical mounting space available.
Published for:APC Algeria
Cela vous a-t-il été utile ?
En savoir plus
En savoir plus