Technical FAQs

Ask a Question

NetBotz 750 | Physical Description

Issue:
   Physical Description of the NetBotz 750

Product Line:
   NetBotz version 5
      - Rack Monitor 750

Environment:
   NetBotz v5.X

Resolution:

Physical Description



 
Item Description
1 AC line inlet Input power connection.
2 Switched Outlet Provides power to a device at a maximum of 10 A. Activates a connected device when configured events occur. (For example, a fan may be connected to this outlet, and the outlet may be configured to turn on when certain alarms are generated.)
3 A-Link ports Provide communications and power to connected devices (sensor pods, rack access pods, and temperature/humidity sensors with digital displays) over standard CAT-5 cabling with straight-through wiring. For instructions to cascade devices, see the Installation and Quick Configuration Manual.
4 Leak Rope ports Used for connecting a NetBotz Leak Rope Sensor (NBES0308).
5 Rack Access Ports* Ports for the door switch sensors (NBES0302 or NBES0303) and handle sensors (NBHN125 or NBHN1356).
6 Universal Sensor ports Used to connect APC by Schneider Electric sensors, third-party dry-contact sensors, and standard, third-party 0-5 V sensors. Third-party, dry-contact state sensors require the NetBotz Dry Contact Cable (NBES0304), and third party, 0-5 V sensors require the NetBotz 0-5 V sensor cable (NBES0305).
7 Beacon Port Used for connecting an Alarm Beacon (AP9324).
8 10/100/1000 Network Port Provides a connection to the network. Status and link Light-emitting Diodes (LEDs) indicate network traffic. See Link LED and Status LED for additional information.
9 Private LAN Provides a 10/100/1000 connection to a private local area network and 48 VDC to an attached device.
10 Wireless Sensor Coordinator USB Port with Wireless NetBotz USB Coordinator (NBWC100U) installed. Used with wireless sensors.
11 USB Type A Ports Reserved for future use.
12 Modbus RS485 Port Reserved for future use.
13 Voltage Output Provides 12 VDC or 24 VDC (75 mA) to one connected device.
13 Relay Output Used for connecting relay-controlled external devices. Relay Outputs can only be connected to Class 2 circuits.
14 4-20 mA Inputs Inputs for industry standard 4-20 mA sensors.
15 Console Port Provides a serial connection to the appliance.
16 Power LED Illuminates when the unit is receiving power.
17 Reset Switch Reboots the appliance.
18 Exhaust fan Exhausts hot air from the appliance.
*Note supported on firmware version 5.0.1. Update the firmware to access these features.
Was this helpful?
What can we do to improve the information ?