Technical FAQs

Ask a Question

Is there a Raven Black spray paint available for NetShelter cabinets?

Issue:
A customer requests spray paint. 

Product Line:
NetShelter SX, SV VX, WX 

Environment:
All versions and serial ranges.

Cause:
Minor damage to the paint may require spray paint to cover. 

Resolution:

We do not currently offer the Raven Black in spray paint, but we do have it available in a paint pen under part #690-0108-001. 
Rust-Oleum has a black spray paint available that, while not a perfect match, can be used. Since it's not a perfect match the painted surface may be visible depending upon the lighting. 
The Rust-Oleum part number is 7220830, Textured Black. 
Was this helpful?
What can we do to improve the information ?