Technical FAQs

Ask a Question

ACRC301S main board interface connections

 
Issue:
ACRC301S main board interface connections.
 
Product line:
ACRC301S, ACRC301H.
 
Environment:
All Serial Numbers.
 
Cause:
Install, Repair.
 
Resolution
 
This is for certified Schneider Electric Field Service Engineer’s
 

Safety information before working on any Schneider Electric Cooling Unit
 
Ensure the refrigerant has been fully reclaimed.
 
Heavy: The compressor is heavy. Do not lift without assistance or a
lifting device.
 
Caution: At the rotolock fittings, use shop rags or
other means to prevent any oil from blowing out of the refrigerant lines.


 
Was this helpful?
What can we do to improve the information ?