Technical FAQs

Ask a Question

Ports used by each component of PowerChute Business Edition.

Issue:
What ports are used by each component of PowerChute Business Edition

Product Line:
PowerChute Business Edition

Environment:
All supported OS

Cause:
Informational

Solution:

TCP
2161 – Communication between Server and Agent (PowerChute 9.2.1 and below)
2160 – Communication between Console and Server (PowerChute 6.x)
2260 – Communication between Console and Server (PowerChute 7.x, 8.x, 9.2.1 and below)
3052 – Agent Web UI and Logging features (PowerChute 9.2.1 and below)
6547 – Agent Web UI (PowerChute 9.x and 10)
 
UDP
2161 – Discovery of Agents by Server (PowerChute 9.2.1 and below)
2160 – Discovery of Servers by Console (PowerChute 9.2.1 and below)
7846 – Business Edition SNMP Agent
 
Was this helpful?
What can we do to improve the information ?