Browse FAQs



What is the difference between an InRow RP, InRow RD (600mm), and InRow RC (600mm)?
The minimum required kW for 1 direct expansion unit is 12kw and 12kw for chilled water . There should also be a consideration regarding humidity control.
What are your humidifier specifications and control operations for the InRow RP?
... between the humidify setpoint and the average return air humidity of all the units in the cooling group (if more than one unit is ...
UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
... , g50 AV Units , Smart- ... acrc301h, acrc301s Cooling Units , ... ap9320 Environmental Monitoring Units FM35XX Network Air , acda901, ... acrc ACRCXXXX InRow Chilled Water (except ACRC3XXX ... ... your local APC Cooling Support team) ... ... ACRP5XX, ACRD5XX InRow RC, RP , RD AOS ... ... your local APC Cooling Support team) acsc ACSC1XX InRow SC AOS v ... ... your local APC Cooling Support team) raru ACFXXX Rack Air Removal Unit AOS v3 ... ACRD1XX, ACRD2XX InRow RD AOS v ... (via your local APC Cooling Support team) nb200 NetBotz 200 Rack Monitor (nbrk0201)
ACSC1XX Spare Parts List
This document contains the Spare Parts List for ACSC1XX units . ... Please contact Cooling Tech Support to confirm the part numbers before quoting as some may have changed. ... Manufacturing # ... CONDENSATE PUMP WIRE ASSY CP JUMPER (for activation without the water sensor kit) ... FITTING 1/8" BARB TEE (for air differential pressure switch) ... Front Door Assembly - Spare Part ... InRow RC/SC Filter 1/2" Washable - Spare Part (default) ... Wire Assembly Base
APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units . APC Unit Identification FM Air / Water /Glycol Air Pattern W= Water Cooled F= Water Cooled D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled ... W= Hot Water Air Pattern ... coil C= Chilled Water Air Pattern C= Chilled Water Air Pattern ... Main C= Chilled Water Air Pattern W= Water Cooled ... G= Glycol Cooled BA=208 ... Air Pattern W= Water Cooled ... G= Glycol Cooled Air Pattern W= Water Cooled
Inrow Chilled Water Units Internal Volumes
Issue: Inrow Chilled Water Units Internal Volumes
acrd200 Water Spec
Cause: Inrow Water Cooled Units Internal Volumes
acrd200 Internal Water Volume
Cause: Inrow Water Cooled Units Internal Volumes
Why is my ACRP excessively cycling?
Data Center Cooling The InRow RP works to prevent ... ... load that the RP is given. ... With the supply air and cool setpoints both at ... In the Inrow configuration, the supply air setpoint controls the temperature of the air the unit supplies to the ... The cool setpoint controls the ... ... relative to the cool setpoint). Setting the cool setpoint between 72 ... and monitoring the unit performance, adjusting the cool and supply air setpoints as needed ... ... will enable the unit to use the ... under "configure unit " on the ... interface under the unit tab, then ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.