Browse FAQs



CDU Spare Parts List
) acac20002 Flexible Fluid Piping Clamp/Hanger (Qty Of 10 ) acac20010 Flexible Fluid Piping Clamp / Hanger ( Qty Of 50
ACRP1XX, ACRD5XX, ACRP5XX, and ACRC5XX Parts List
... Meters) acac20003 Flexible Fluid Piping - 300 Feet ... Meters) acac20002 Flexible Fluid Piping Clamp / Hanger acac20007 Flexible Fluid Piping Clamp / Hanger ( qty of 50 ) acac20008 Flexible Fluid Piping Couplings (4 ...
What are the operational conditions for an InRoom (Stulz) Unit
... /cooling water pipes : ... equivalent length of piping between the cooling ... ... °F) 50 % R. ... Return air conditions for cooling capacity (CW): 24°C (75°F) 50 % R.H. ... Cooling fluid (DX): 30% Glycol Fluid inlet temperature (G): 30°C (86°F) Fluid outlet temperature (G): 40°C (104°F) ... Upflow units with an external static pressure: 50 Pa (0.20 in w g)
How to navigate through an Network Air FM unit display
Settings for fluid -cooled options ... the valve and piping settings must be ... each type of fluid -cooled option ... The condenser fluid valve controls the ... ... Set the condenser fluid valve as a ... Coil Fluid . The coil fluid valve controls the ... ... Set the coil fluid valve as a ... ... no external water piping do not require ... Coil Fluid . ... Set the coil fluid valve actuator to ... ... Config > Coil Fluid Options ... in the coolant piping for this System ... Coil fluid temperature activation threshold ... ... Config > Coil Fluid Options The Coil Fluid Options Coil Fluid Temp Activation: ...
ACSC1XX Spare Parts List
QTY ... COMP Assy, SC, ROTARY 220-240/1/ 50 (Toshiba conversion kit ... COMP, ROTARY 220-240/1/ 50 SC, TOSHIBA - SPARE PART ... TUBE 6 FT 10" DIA FLEX DUCT ... 1U Airflow Management Blanking Panel Kit ( Qty 2) Black ... 1U 19" Black Modular Toolless Airflow Management Blanking Panel - Qty 10 ... 1U 19" Black Modular Toolless Airflow Management Blanking Panel - Qty 200
Refrigerant charging table for a Uniflair Unit
... • All refrigerant piping is type L ... ... /chilled water piping are free from ... ... • All refrigerant piping joints must be ... ... • All refrigerant pipes are installed with ... approved refrigerant line clamps . Isolate piping from structural surfaces ... /AC vibration clamps . ... length of a pipe run. ... the diameter of pipe : • For pipes running in a ... direction, select pipe size from the ... ... below to determine pipe diameter for vertical pipes . ... 15 m ( 50 ft). • Use the table below to determine pipe diameter for horizontal pipes . ... 2. Connect a vacuum pump to the service ports on the system piping .
What is the flow rate required for the InRow acrd20x fluid-cooled unit?
This is for a single acrd20x piped to a single outdoor fluid cooler.
What is the flow rate required for the InRow ACRD2XX fluid-cooled unit?
This is for a single RD piped to a single outdoor fluid cooler.
What does “equivalent pipe length” mean?
Equivalent pipe length, is ... , fittings and fluid velocities to a representative length of straight pipe of a stated type (metal, plastic ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.