Browse FAQs



CDU Spare Parts List
) acac20003 Flexible Fluid Piping (300 Feet 91.4 Meters ) acac20002 Flexible Fluid Piping Clamp / Hanger (Qty Of 10
ACRP1XX, ACRD5XX, ACRP5XX, and ACRC5XX Parts List
... Meters) acac20003 Flexible Fluid Piping - 300 Feet ... Meters) acac20002 Flexible Fluid Piping Clamp / Hanger acac20007 Flexible Fluid Piping Clamp / Hanger (qty of 50) acac20008 Flexible Fluid Piping Couplings (4 ...
What is the flow rate required for the InRow acrd20x fluid-cooled unit?
This is for a single acrd20x piped to a single outdoor fluid cooler.
What is the flow rate required for the InRow ACRD2XX fluid-cooled unit?
This is for a single RD piped to a single outdoor fluid cooler.
What does “equivalent pipe length” mean?
Equivalent pipe length, is ... , fittings and fluid velocities to a representative length of straight pipe of a stated type (metal, plastic ...
What does “Equivalent Pipe Length” mean?
Equivalent pipe length, EPL ... , fittings and fluid velocities to a representative length of straight pipe of a stated type (metal, plastic ...
What are the placement considerations for the fluid cooler relative to the InRow acrd20x?
The fluid cooler can be placed up to 600ft equivalent pipe length from the unit.
What are the placement considerations for the condenser relative to the InRow RD? What are the other factors involved with purchasing a fluid cooler?
The fluid cooler can be placed up to 600ft equivalent pipe length from the unit. A definition of equivalent pipe length has been provided above.
What are some of the applications for the InRow ACRD?
... to install the same unit in different applications as a result of flexible heat rejection options like air and fluid based.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.