Search FAQs
NetBotz 750 | How do I connect serially?
Issue:
How do I serially connect to the NetBotz 750?
Product Line:
NetBotz version 5.X
Environment:
NetBotz v5.X
Cause:
Serial parameters and drivers are required to establish a serial connection between a computer and the NetBotz appliance.
Resolution:
The NetBotz 750 uses the following serial parameters:
- Baud Rate: 115200
- Data Bits: 8
- Parity: None
- Stop Bits: 1
- Flow Control: None
To log in and configure the 750 with an IP, you will need to log in with root as the user and you will be prompted for a password.
If you connect your NetBotz 750 to your computer and do not see it show up as a serial port (unknown device), you need to download the driver:
Serial port driver - Silcon Labs CP2103
https://www.silabs.com/products/development-tools/software/usb-to-uart-bridge-vcp-drivers
How do I serially connect to the NetBotz 750?
Product Line:
NetBotz version 5.X
Environment:
NetBotz v5.X
Cause:
Serial parameters and drivers are required to establish a serial connection between a computer and the NetBotz appliance.
Resolution:
The NetBotz 750 uses the following serial parameters:
- Baud Rate: 115200
- Data Bits: 8
- Parity: None
- Stop Bits: 1
- Flow Control: None
To log in and configure the 750 with an IP, you will need to log in with root as the user and you will be prompted for a password.
If you connect your NetBotz 750 to your computer and do not see it show up as a serial port (unknown device), you need to download the driver:
Serial port driver - Silcon Labs CP2103
https://www.silabs.com/products/development-tools/software/usb-to-uart-bridge-vcp-drivers
Released for:APC South Africa
Explore more
Explore more