Technical FAQs

Ask a Question

PowerChute Business Edition v10.0 Agent UI does not launch

Issue:
The PowerChute Agent web user interface (UI) does not launch using Google Chrome or Mozilla Firefox.

Product Line:
PowerChute Business Edition v10.0

Environment: 
Google Chrome v
70+ and Mozilla Firefox v64+

Solution 1 (Google Chrome only):

In Google Chrome, type chrome://flags in the address bar and hit Enter. Disable TLS 1.3 from the list of options. The PowerChute UI will successfully launch when TLS 1.3 is disabled.
 
Solution 2 (applicable to both Chrome and Firefox):

Launch the PowerChute Agent UI in an alternative browser (e.g. Microsoft Edge). Upgrade the Java version used by PowerChute to OpenJDK v11.0.1, available to download on the OpenJDK website.
 
When the Java upgrade has successfully completed, launch the PowerChute Agent UI in Chrome or Firefox.
 
Was this helpful?
What can we do to improve the information ?