Video: How to verify USB communications between UPS and Windows OS using UsbDeview.exe
Published date:
25 March 2019
Issue:
need to check USB communications between Windows OS and APC Back-UPS or APC Smart-UPS
NOTE: The USB drivers for communications between APC UPS and Windows OS are pre-installed in the Windows OS.
The drivers should load automatically once the APC UPS has been connected to the computer using the proper USB cable.
If the drivers do not load automatically once the USB cable has been connect to the UPS and the computer open C:\Windows\System32\drivers and verify that
hidclass.sys, hidparse.sys, and hidusb.sys are available. Also verify that apcups.inf is available in C:\Windows\System32\DriverStore\FileRepository
Product Lines:
Back-UPS and Smart-UPS that accept USB communications
PowerChute Personal Edition
PowerChute Business Edition
Environment:
All supported Windows OS
Cause:
Testing USB communications using UsbDeview.exe
Solution:
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.