Browse FAQs

Can not change write community string for NBRK0750, NBWL0755

Published date: 29 October 2019

Issue:
Can not change NetBotz version 5.2 write community string.

Product Line:
NetBotz

Environment:
NBRK0750, NBWL0755
NetBotz 5.1, 5.2

Cause:
The write community name is only used when working with StruxureWare DCE at this stage. It was added in as a default to be able to work with DCE's priority scanning feature.
The UI was not initially updated to allow for editing of this field.

Resolution:
Version 5.2.1 is slated to have an edit field for this setting.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.