Consultar las preguntas frecuentes

NetBotz 250 | Physical Description

Fecha de publicación: 20 May 2020

Issue:
   Physical Description of the NetBotz 250.

Product Line:
   NetBotz Rack Monitor 250 (NBRK0250)

Environment:
   NetBotz Rack Monitor 250 (all versions)

Resolution:

Physical Description



 
Item Description
1 AC line inlet Input power connection.
2 Switched Outlet Provides power to a device at a maximum of 10 A. Activates a connected device when configured events occur. (For example, a fan may be connected to this outlet, and the outlet may be configured to turn on when a high threshold violation occurs for a temperature sensor.)
3 Wireless Sensor Network USB port with NetBotz USB Coordinator (NBWC100U) installed. Used with included Wireless Temperature Sensor (NBWS100T) to monitor temperature. Additional wireless sensors can be purchased separately. 
4 Rack Access Ports Ports for the door switch sensors on doors #1 and #2.
Ports for the handle sensors (NBHN125 or NBHN1356) on doors #1 and #2.
5 Beacon Port Used for connecting an alarm beacon (AP9324).
6 Universal Sensor ports Used to connect APC by Schneider Electric sensors and third-party dry contact sensors. Third-party dry contact sensors require a Dry Contact Cable (NBES0304).
7 USB Port Used to connect USB devices to the appliance.
8 Voltage Output Provides 12 Vdc or 24 Vdc (75mA) to a connected device.
Relay Output Used for connecting relay-controlled external devices.
9 10/100 Network Port Provides the connection to the network. Status and link Light-emitting Diodes (LEDs) indicate network traffic. See Link LED and Status LED for additional information.
10 A-Link Ports Used to cascade NetBotz Rack Sensor Pod 150s (NBPD0150), or connect Temperature/Humidity Sensors with Digital Display (AP9520TH). Provides communications and power using standard CAT-5 cabling with straight-through wiring.
NOTE: To cascade multiple devices, connect a supplemental power supply (100-240 Vac/24 Vdc, part number AP9505i) to a NetBotz Rack Sensor Pod 150.
11 Modbus RS-485 port Provides the connection to a building management system using the Modbus protocol.
12 Console Port Used to connect the USB A-USB mini B configuration cable, when configuring initial network settings.
NOTE: See knowledge base FA381239 for instructions on configuring the network settings (TCP/IP) and knowledge base FA381275 for instructions on installing the required FTDI VCP driver.
13 Power LED Indicates whether the unit is receiving power (blue = receiving power; dark = not receiving power).
14 Reset button Restarts the Rack Monitor 250 network management interface.

¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.