Consultar las preguntas frecuentes

SRT 8 or 10kVA experiences excessive battery transfer and re-transfer events in 3 phase systems

Fecha de publicación: 27 August 2020

Issue: The UPS experiences excessive battery transfer/retransfer events in 3PH systems.

Product Line:
SRT 8-10kVA Models
 
Resolution:
Clear the Alarm. Turn the output ON again. If the problem persists, Brain dead the UPS. If the alarm reoccurs, perform a UPS Firmware upgrade to the latest 04.7 revision that addressed these issues. For complete upgrade instructions please refer to FA164737.
 
Release Notes (UPS 04.7):
========================
1. Improved system performance of transitions between Online and Bypass operation modes.
2. Improved system behaviour for three phase input configurations to reduce transitions to battery under certain input feed conditions.
3. Improved system behaviour to eliminate false detection of DC bus under voltage alarm under certain conditions.
4. Improved system handling for certain AC input conditions during system start-up.
 

¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.