Consultar las preguntas frecuentes

StruxureWare | Can I install Data Center Expert on my own server?

Fecha de publicación: 16 July 2020

Issue:
StruxureWare Data Center Expert (DCE) is only supported on hardware provided by APC /Schneider Electric

Product Line
StruxureWare Data Center Expert (DCE)
- Basic Appliance (AP9465)
- Standard Appliance (AP9470)
- Enterprise Appliance (AP9475)
- Virtual Appliance (AP94VMACT)
StruxureWare Central (SWC)
InfraStruXure Central (ISXC)

Environment:
StruxureWare Data Center Expert 7.x and earlier

Cause:
StruxureWare Data Center expert is a highly customized operating system.

Resolution:

StruxureWare Data Center Expert (DCE) is not supported as in install directly on any 3rd party hardware. There are specific drivers that are included in the system and we will not properly install on any hardware other than those sold by APC / Schneider Electric. Additionally, the install limits the amonts of devices that can be monitored based on the hardware on which it is installed.

If you must use 3rd party hardware, you can install VMware on that hardware and use the AP94VMTRL trial version of DCE and activate it using the AP94VMACT. With that, you have your own hardware as well as a supported system for running StruxureWare DCE in a virtual environment.
 

¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.