Consultar las preguntas frecuentes



Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... , Smart- UPS Online (SRT ... ... device from v 5 .X. ... contact APC Technical Support in ... ... installed in a UPS , you need to determine which UPS you have. APC offers several different UPS families. Smart UPS ... Select the correct UPS or device type ... ... /www. apc .com/ ... ... have a Smart UPS 750 (sua750 ... ... executable for Smart UPS and Matrix w ... ... Management Card v 5 .X. ... executable for Smart UPS w/ap9630 ... ... AP9631 use version 5 .X or ... ... only on the APC public FTP site ...
Matrix-UPS frequently asked questions regarding installation, operation, and standards
... about the Matrix UPS ? Matrix UPS ... of a Matrix UPS . ... installation of the APC Matrix UPS . ... . Matrix- UPS should be set ... ... to know input voltage to Matrix- UPS . ... , Matrix- UPS Input Select Tap ... ... Set Matrix- UPS EU (Electronics ... of Matrix- UPS IU (Isolation ... ... of Matrix- UPS or by its ... 5 . Hook Anderson ... ... of Matrix- UPS IU to " ... ... 7. Front LCD display should read ... If LCD display does not ... ... option of the LCD display to check current Matrix- UPS settings.
Changing the Language of the Symmetra PowerView RM Display
Smart- UPS VT Smart- UPS RT 15/ ... ... or at the APC Web site ( ... /www. apc .com) ... ... or at the APC Web site. ... RM from the UPS . ... (included, APC part number 940 ... RM and the UPS data cable: ... or to the APC Web site. c . Attach the UPS data cable to ... ... available on the APC Web site. 5 . Place the ... The LCD will display the ... To leave the Programming screen ... ... by repeating steps 5 and 6. ... and reconnect the UPS data cable to ... 8. Affix the PowerView RM to the UPS .
Video: How can I download Event, Data, Configuration, and Debug files from my Network Management Card?
... , Smart- UPS Online (SRT ... ... txt, select UPS debug files ( ... Please follow the procedure below for FTP instructions on v3.X.X, v 5 .X.X, and v6.X.X firmware versions. ... 5 .) Type bin ... 13.) Type bye and exit out of your command prompt or FTP client. ... 5 .) For config.ini ... apc >logzip ... apc ... 230 User logged in, proceed. ... (This can be done by using the LCD ftp command.)
Video: How do I troubleshoot the Replace Battery LED on a Smart-UPS?
... my Smart- UPS . Smart- UPS , Smart- UPS Online ... , or the LCD Screen on the UPS (if so ... ... for a standard UPS or 24 hours for a UPS with external batteries ... Smart- UPS products will charge ... If your UPS has an LCD screen go to the ... then select " UPS Self Test" If your UPS does not have an LCD display, press ... ... last 3- 5 years, however ... >25° C / 77° ... ... all Smart- UPS products is 2 ... contact APC Customer Support
Video: How do I configure APC Network Management Card network settings?
... , Smart- UPS Online (SRT ... ... , all of APC's Network Management Card ... ... , all of APC's Network Management Card ... All APC devices have a ... begin with 00 C 0 B7 Smart- UPS front panel LCD - (available ... ... to download from APC's website ... beginning with 00 C 0 B7 ... which indicates an APC address. ... , available from apc .com, ... ... serial version of APC's PowerChute software, the APC UPS service must be ... ... properly with an APC UPS or accessory. ...
How can I adjust the number of battery packs on a Smart-UPS XL?
Smart- UPS XL products require ... you tell the UPS how many external ... so that the UPS can properly calculate ... Smart- UPS XL Smart- UPS XL models are ... Smart- UPS XL models are ... ... a Smart- UPS performs when it ... the Smart- UPS XL to recognize ... ... . First, EXIT out of the ... the UPS service must be ... 5 . Click on ... ... properly with an APC UPS or c . Type " ... ... com port the UPS serial c . Type " ... ... PowerChute plus version 5 .x for ... PowerChute plus 5 .x for ...
What is the expected life of my APC UPS battery?
If the ambient temperature during storage is - 15° C to + 30° C (+ 5 °F to + 86° ...
Why is my equipment dropped or rebooted while connected to my Smart-UPS?
... to Smart- UPS drops or reboots ... Smart- UPS ... a Smart- UPS can be dropped ... - A UPS with a weak ... ... Every Smart- UPS has a " ... ... last 3- 5 years in a ... C (68- ... C (15 C (77 C (95 ... failure which the UPS self test may ... ... result in unexpected UPS behavior including load drops and the UPS turning off: - Each UPS is limited in ... ... number of the UPS tells you the Volt -Amp ( ... ... up to 1000 Volt Amps (or ...
Can I use a domestic model UPS in a foreign country?
APC's international models have an input requirement of 230 volts , 50-60hz and an output of 230 volts 50-60hz.


Resultados 1 - 10 de 71

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.