Consultar las preguntas frecuentes



Smart-UPS C Series FAQ
Smart-UPS C Series FAQ Smart-UPS ... is the new Smart-UPS C series? The Smart-UPS C series is ... new entry level Smart-UPS product designed for ... ... feature a new LCD Interface. ... dedicated Tower or Rack -Mount models ... ... 1500va in both Rack and Tower form ... ... America use NEMA 5 -15 plugs ... ... with the SMC Smart-UPS ? The SMC Smart-UPS supports Powerchute Business ... ... not have a Smart -Slot and ... Is the LCD display the same ... SMT and SMX Smart-UPS products?
What are the Minimum and Maximum mounting depths for Smart-UPS rails?
Issue: What are the Minimum and Maximum mounting depths for Smart-UPS rack mount rails?
Video: How do I configure a 208v Smart-UPS RT or SRT for use with a 240v input?
... configure a 208v Smart-UPS RT or SRT ... Smart-UPS Online (RT ... Smart-UPS RT and SRT ... The Smart UPS Online line has ... of acceptable input voltages , and as ... ... avoid a sudden voltage shift in the event that the UPS goes to bypass ... to configure the UPS output to match the UPS input. ... turn off the UPS . ... would select the UPS ... . On the UPS tab we would ... ... Here we choose 240 VAC output and ... The UPS will now output ... Output voltage will not change if the UPS is left "on" ...
Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
... information of the UPS operation condition such ... input/output voltage , input/ ... , and battery voltage , etc.,The Output Voltage can be set through LCD : 220 / 230 / 240 Vac.
Video: How do I configure APC Network Management Card network settings?
Return to Top Configuration Method 5 - via Smart-UPS front panel LCD - (Supported SMT, SMX, and SRT
Installing Standard APC Rails to a Threaded Rack
Product Line: Smart-UPS , Smart-UPS Online
Are the NetShelter VX Seismic cabinets and 2-Post Racks OSHPD compliant?
Several Smart-UPS were tested and approved for installation with NetShelter VX Seismic and ar201 during OSHPD Special Seismic Preapproval (OSP) testing ...


Resultados 1 - 10 de 72

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.