Consultar las preguntas frecuentes



Video: How can I download Event, Data, Configuration, and Debug files from my Network Management Card?
... , Smart- UPS Online (SRT ... ... txt, select UPS debug files ( ... ... X, v 5 .X. ... 5 .) Type bin ... 13.) Type bye and exit out of your command prompt or FTP client. ... 5 .) For config.ini ... apc >logzip ... apc 331 User name okay , need password. ... 230 User logged in, proceed. ... 200 TYPE Command okay . ... 250 CWD requested file action okay , completed. ... 200 PORT Command okay . 150 File status okay ; about to open data connection. ... 150 File status okay ; about to open data connection.
Video: Why might my APC Back-UPS Product be beeping?
APC's UPS Selector ... indicates that the UPS has detected an ... ... determine if your UPS is capable of ... 5 .) Disabling UPS audible alarm tones ... ... software, the UPS audible alarm tones ... ... 1 beep every 5 seconds ... If the input voltage is determined to ... equipment, the UPS will transfer to ... ... for the acceptable voltage window. The UPS is trying to ... ... unit shipped with APC management software it ... the default acceptable voltages that the unit ... ... section of the APC management software for ... ... + or - 5 % this will ... ... is 3 to 5 times the size ...
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... , Smart- UPS Online (SRT ... ... device from v 5 .X. ... contact APC Technical Support in ... ... installed in a UPS , you need to determine which UPS you have. APC offers several different UPS families. Smart UPS ... Select the correct UPS or device type ... ... /www. apc .com/ ... ... have a Smart UPS 750 (sua750 ... ... executable for Smart UPS and Matrix w ... ... Management Card v 5 .X. ... executable for Smart UPS w/ap9630 ... ... AP9631 use version 5 .X or ... ... only on the APC public FTP site ...
How can I adjust the number of battery packs on a Smart-UPS XL?
Smart- UPS XL products require ... you tell the UPS how many external ... so that the UPS can properly calculate ... Smart- UPS XL Smart- UPS XL models are ... Smart- UPS XL models are ... ... a Smart- UPS performs when it ... the Smart- UPS XL to recognize ... ... . First, EXIT out of the ... the UPS service must be ... ... and then click OK . 5 . Click on ... ... 6. Click OK twice. ... properly with an APC UPS or ... com port the UPS serial ... PowerChute plus version 5 .x for ...
What are the basic troubleshooting steps for the APC Back-UPS Pro with Networking bg500 ?
... steps for the APC Back-UPS ... APC Back-UPS ... ... find the your APC AV J- ... ... brownout or over voltage condition. ... cold boot the UPS when no AC ... The UPS will not cold ... ... is restored the UPS can be turned ... Contact APC Technical Support for ... Leave the Back- ... Contact APC at the Web site www. apc .com, ... ... Cannot find the UPS IP when searching ... ... Cannot find the UPS IP when searching ... Make sure the UPS and your PC ... ... : If the UPS connected to a ...
Can I use a domestic model UPS in a foreign country?
APC's international models have an input requirement of 230 volts , 50-60hz and an output of 230 volts 50-60hz.
Symmetra LX Spare Parts List
... parts for the APC Symmetra LX UPS system? ... a Symmetra LX UPS . APC Symmetra LX Battery ... APC Symmetra LX Battery ... APC Symmetra LX Intelligence ... ... Castor kit - left front, right ... ... right front, left rear - SYAFSU7 APC Symmetra LX XR ... APC Symmetra RM XR ... APC Symmetra LX XR ... APC Symmetra LX 5 U replacement door ... ... For 220/ 230 /240/ ... APC Symmetra LX Battery ... APC Symmetra LX Intelligence ... ... Castor kit - left front, right ... ... right front, left rear - SYAFSU7 APC Symmetra LX XR ... APC Symmetra RM XR ... APC Symmetra LX XR Communication Cable - 0w6002b APC Symmetra LX 5 U replacement door - SYAFSU1
What are the basic troubleshooting steps for the Back-UPS Connect model bg500?
APC Back-UPS ... ... brownout or over voltage condition. UPS will not turn ... cold boot the UPS when no AC ... The UPS will not cold ... ... is restored the UPS can be turned ... Contact APC Technical Support for ... Leave the Back- ... Contact APC at the Web site www. apc .com, ... ... Cannot find the UPS IP when searching ... Make sure the UPS and your PC ... ... : If the UPS connected to a ... ... the network IP to DHCP mode, both user name and password to " apc ", clear and reset all the web configuration to ...
Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
... can get the clear and correct information of the UPS operation condition such ... input/output voltage , input/ ... , and battery voltage , etc.,The Output Voltage can be set ... : 220 / 230 / 240 Vac ...
Video: Configuring clearing events with APC Network Management Cards
... do I configure clearing events on the ... ... X, v 5 .X. ... ... such as " UPS : Passed Self ... ... referred to as clearing events. A clearing event notification is ... certain condition is cleared so to avoid ... UPS : On battery ... clearing event is Informational ... UPS : No longer ... ... notified when the UPS goes to battery ... and if the UPS comes off of ... UPS : No longer ... ... the Critical - UPS : On battery ... ... but not the clearing event - Informational ... UPS : No longer ... ... think that the UPS is still on ...


Resultados 1 - 10 de 90

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.