Consultar las preguntas frecuentes



NetBotz Temperature Sensors are NOT Thermocouples
The temperature sensors used on NetBotz Devices and NetBotz manufactured externals sensors are not thermocouple devices. NetBotz utilizes semi-conductor devices for temperature measurement.
Wiring specifications for NetBotz Dry Contact Cables
Resolution: 24 gauge wire is used in the NetBotz manufactured dry contact cables.
Why does my 0-5V analog input on my NetBotz appliance read twice what it should?
... the potential for some nbac0231 cables to have been incorrectly manufactured , and as a result will provide measurements to the NetBotz device that are ...
MAC address Vendor ID of Network Management Cards, and other network devices changing
Netbotz devices (rack/wall mount, mini sensors) ... A MAC address is a unique identifer given to a network card when it is manufactured . ... Units manufactured in late Q4 2017 will have the new MAC prefix.
Humidity Sensor Issue with 300/303/310/400 Series Appliances
NetBotz NetBotz version 1 NetBotz has discovered a ... some of our NetBotz environmental monitoring appliances ... ... only some older NetBotz hardware versions. ... determine if your NetBotz appliance is affected ... ... No currently shipping NetBotz appliances are affected ... ... when it was manufactured or purchased, ... ... sensor to generate NetBotz alert notifications) ... was discovered, NetBotz released a BotzWare ... ... needs of most NetBotz customers. ... thresholds above 60% or if you have any other concerns, please call NetBotz Support toll free at 1-877-908-2688 and the NetBotz Support Team will work with you to determine ...
Why can't I connect to my APC Network Management Card or embedded Network Management Card using a serial connection?
Devices with an embedded Network Management Card 1 include (but are not limited to): Metered/Switched Rack PDUs (AP78XX, AP79XX), Rack Automatic Transfer Switches (AP77XX, Environmental Monitoring Units (ap9320, ap9340, Netbotz 200) ... There are several different communication cables APC manufactures .
Reformatting a 300/303/310/400 Series Appliances
NetBotz ... NetBotz version 1 ... NetBotz ROM Version 1.3.34 ... Manufacture Date: 10/30/2001


Resultados 1 - 10 de 70

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.