Consultar las preguntas frecuentes



Where can I get support for APC and MGE Products?
... 50 0031- 10 0031-6 0033- 10 0033-25 ... 6 0034- 1 0034-100 ... 100 0035- 2 M-E ... E 0035nd- 2 M- 1 E 0035nd-3M- 1 E 0039-15 0040- 10 0040-15 ...
Network Air FM unit spare parts list
ADAPTER ROTO 1 1 /4" ... ADAPTER ROTO 1 "-14R ... ... CAT5 for EXP unit ... BKR 3P K 16A 480y/ ... ... BKR 3P K 20a 480y/ ... ... - MKC- 1 ... - MKC- 2 ... -30- 10 -81 ... -30- 10 -81 ... (compressor [ K 1 & K 2 ]) ... -30- 10 -81 ... (humidifier [ K 3] & heater [ K 4]) ... -30- 10 -81 ... DF 5/ Unit 756 X 325 ... ... DF 5/ Unit 756 X 325 ...
Symmetra PX 250/500; AP9635; Flood of RTC Time adjusted values in the logs
... value Parallel UPS 1 2 02-26 ... Time old value 2 02-28-2015 17:12:57 446 46931 Info
What's the difference between seismic Zone 4 maps and High Seismic Area maps? Can one be substituted for the other? Which cabinet should I choose?
Generally, over the past two decades , building codes have replaced maps having numbered zones with maps showing contours of design ground motion.
Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
... ,8 and 10 KVA FAQ ... SRC 5- 10 KVA UXI Models ... ... to connect the two UPSs' output ... Both the UPSs share the load equally but if one fails (either through developing a fault or being taken out of service for maintenance), the other UPS will take over powering the load. ... Q: What are the advantages of the SRC 5- 10 KVA LCD Display? ... A: In addition to the 1 + 1 Parallel redundancy system, the Customer can also look into a service bypass panel which will give you a wrap around bypass.
Symmetra PX1-PX2; How to interpret the loading displayed in Symmetra PX
How to interpret the loading displayed in Symmetra PX ... The opening screen of Powerview shows loading of the heavily loaded phase in Symmetra PX . ... Typical loading data from Symmetra PX unit is give below as an example ... L 1 ... L 2 ... 2 A 10 %
Serial communications between Smart-UPS VTs, Galaxy 3500, and Symmetra PX with IBM AS/400, i Series
... , and Symmetra PX with IBM AS ... FA159551 K -Base. ... ... 3500, Symmetra PX , or other ... If the UPS has two or more SmartSlots, you can refer to for the proper installation order of multiple accessories. ... If the NMC is needed and your UPS only has one SmartSlot, attach expansion chassis part numbers ap9600 or ap9604blk to the serial port of the UPS and install the NMC in the chassis.
EcoBreeze Variable Speed Drive Technical Spec’s
R2B configurable relay logic NC , electrical durability 100000 cycles Minimum switching current R 1 -R 2 10 mA at 5 V DC
NetBotz Rack Access PX - HID (AP9361) | How do I configure RADIUS authentication for my card reader?
... NetBotz Rack Access PX -HID? ... - Rack Access PX -HID ( ... ... - Rack Access PX -HID ( ... ... NetBotz Rack Access PX - HID ( ... ... NetBotz Rack Access PX Basic (ap9360 ... ... NetBotz Rack Access PX . ... Service-Type 1 integer APC ... APC-Outlets 2 string APC ... ACCPX-access3 10 string APC VALUE APC-Service-Type Admin 1 VALUE APC-Service-Type Device 2 ... Once the RADIUS server has been configured, you can enable RADIUS authentication on the NetB otz Rack Access PX (AP9361). ... - Rack Access PX -HID Only ... - RADIUS, then Rack Access PX -HID
SurgeArrest - minimum install distance of 10 meters (30ft).
Type 1 , 2 , 3 Component Assemblies - Consist of a Type 4 component assembly with internal or external short circuit protection.


Resultados 1 - 10 de 84

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.