Consultar las preguntas frecuentes



​Information for Noise level of UPS Galaxy 5000 NAM
UPS rating ( kVA ) 40/ ... Noise level on a normal floor (dBA) with an RL load at 3 feet 65 63
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
The instructions to power down the UPS are available on the display. This procedure is for a single UPS with an external maintenance bypass panel.
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
The instructions to power down the UPS are available on the display. This procedure is for a single UPS without an external bypass panel.
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from total power ... Galaxy 5000, Galaxy 5500 ... reasons, the Galaxy 5000 may be in a totally off state ... ... not for commissioning a new UPS . ... The commissioning of a new UPS must be performed by a Schneider Electric trained ... ... to restore the Galaxy 5000 UPS from total power ... ... procedure is for a single UPS without an external ... Step 1 : Set the input Q 1 switch to On ... end of the UPS initialization with PFC start -up. ... : Choose “ Start the UPS ... Green “Inverter Start Button”
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
... – STS, Galaxy 3000, 4000 , 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000 , 5000 and Galaxy PW ... , N and 1 . Slave address is 1 and wiring is ... ... This assumes only one 66061 card or UPS or STS is ... ... Monitoring Enclosure has a CB, power ... One is down ( ... ... Modbus card has a female DB9 so a male DB9 cable ... required on the UPS /STS. The male DB9 connector is not supplied with the UPS but a black terminal block is supplied with the EGX.
Video: How to download display export log on a Galaxy VM
Resolution: Start from the UPS Home screen.
Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
1 .) Purchase a right angle DB25 Male-Female interconnection knowledge base article ID
Information for Noise level of UPS Galaxy PW
UPS rating in KVA 100 130 150 180 200 225 Noise level on normal floor (dBA) 62 63 64 65 67 68
Video: Changing the display Language, Date Format & Temperature Units on a Galaxy VM
Configuring Display Language, Date & Temperature Units on Galaxy VM UPS ... Galaxy VM ... Depending on application, the UPS display may need to be adjusted to conform to local language and formatting. ... Go through the steps to change the display settings on a Galaxy VM. Start from the Home screen


Resultados 1 - 10 de 65

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.