Consultar las preguntas frecuentes



MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... for 9600, 8 , N and 1 . Slave address is 1 and wiring is ... ... This assumes only one 66061 card or UPS or STS is ... One is down ( ... ... required on the UPS /STS. The male DB9 connector is not supplied with the UPS but a black terminal block is supplied with the EGX.
What is the expected life of my APC UPS battery?
... , smart- ups , overload, ... , Smart- Ups VT, Galaxy 3500, PX2 ... PX 250- 500 , Galaxy , PW, ... , EPS, VX , VM, ...
Where can I find Modbus Register map for Galaxy VX UPS products
Issue: Where can I find Modbus Register map for Galaxy VX UPS products
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
Turn on the CB1 breaker. Step 8 : Unlock CB2, remove the key, and place it in the key interlock.
How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX?
... ) circuit to Galaxy VX ? Galaxy VX ... ) circuit to Galaxy VX ? ... A35JB8_R 1 _EN. ... When the UPS is EPO'd, ... ... option in the UPS Tuner ( software) to have the UPS go to static bypass on EPO (default setting is no). ... The UIB ( Unit Input Breaker) is not tripped. Tripping of the upstream breaker could be a code requirement, typically if UPS is located in the data center. ... Note; in parallel systems, only the UPS in which the EPO is activated is affected; remaining UPS will still be powered.
Where do I find an Operation Manual for Galaxy VX Series UPS?
Issue: Operation Manual for Galaxy VX Series
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
The instructions to power down the UPS are available on the display. This procedure is for a single UPS without an external bypass panel.
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from total power ... Galaxy 5000, Galaxy 5500 ... reasons, the Galaxy 5000 may be ... ... commissioning a new UPS . ... of a new UPS must be performed ... ... to restore the Galaxy 5000 UPS from total power ... ... is for a single UPS without an external ... Step 1 : Set the input Q 1 switch to On ... end of the UPS initialization with PFC ... Step 4: Choose “Start the UPS ” ... Step 8 : Set the battery circuit breaker(s) QF1 to the On Position. ... The Inverter Assumes the load, and the UPS is normal operation with the load protected.
Smart-UPS VT-Galaxy 3500; Bypass Not Available Input Freq/Volt Out Of Range, Output: Inverter sync. to bypass alarms
Smart- UPS VT- Galaxy 3500; Bypass ... Smart- UPS VT- Galaxy 3500-ais3000 ... occurs when the UPS is online, ... , the UPS should not allow ... to command the UPS to bypass. If the UPS allows you to ... As long as the Mains frequency is inside that window, the UPS should be in normal operation. ... 60 HZ +/- 0, 1 % ... 50 HZ +/- 0, 1 % ... NAM 208v MAX = 228. 8 ... When AC mains returns you may get a informational event for; Mains no longer prevents UPS from switching to bypass.


Resultados 1 - 10 de 54

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.