Consultar las preguntas frecuentes



How to set self test day and time on Symmetra UPS products
Symmetra PX , Symmetra PX2, Symmetra LX, Symmetra RM ... 1 ) A UPS load on command. ... Setup (enter) ... *in the Symmetra PX 48, 100, 160 kVA the menu path is: ... *the self test schedule (interval) can also be adjusted through the network interface. ... If an extended power outage causes your UPS to fully drain batteries and shutdown, the self test day/time will be reset to when the UPS is turned back on.
Input Circuit Breaker Requirements for Symmetra PX 20/40/80 kw
This document describes the required input over current protection (circuit breaker) required when installing a Symmetra PX ... Input Circuit Breaker Requirements for Symmetra PX 20/40/80 kw ... ISX 20k (All-in- One ) ... Symmetra PX 40 ... Symmetra PX 80 ... (APC Symmetra PX Frame Installation Deviation and Selection of Input Circuit Breaker Ratings)
Why does Symmetra LX see only half of my installed battery modules?
The bottom intelligence module monitors battery bays 1 , 3, 5, 7, 9, 11 & 13 while the top intelligence module ...
Can I install multiple APC SmartSlotAccessory Cards in one UPS?
Can I install multiple APC SmartSlotAccessory Cards in one UPS? Symmetra PX (excluding PX 250/500 ... ... may only offer one SmartSlot. ... cards to be installed , this articles ... APC does manufacture a SmartSlot Expansion ... You can daisychain multiple Expansion Chassis units off of one UPS. ... http://www.apcmedia.com/salestools/ASTE-6Z5QFC/ASTE-6Z5QFC_R 1 _EN.pdf Please see the following link for installing multiple SmartSlot accessories in a supported UPS system:
What is the maximum number of XR frames allowed with a Symmetra PX 20, 40 and 80kw solution?
Symmetra PX ; What is ... with a Symmetra PX solution? Symmetra PX 20, 40 ... ... with a Symmetra PX solution is 4 ... ... of the Symmetra PX Main Frame. ... For a Symmetra PX 20 or 40kw ... fully populated ( Battery Frames) XR ... ... a runtime of 1 hr 40 mins ... The Battery Monitoring Card cannot ... ... frame with 8 Batteries Modules. ... There are 4 Battery Units in a ... frame with 32 Battery Units installed . ... For a Symmetra PX 80kw Frame, ... ... total of 4 battery frames in addition ... ... frame with 8 Batteries Modules.
Where do I find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC, and/or the SE modular batteries such as GVSBTU, GVSBTHU and GVSBTHULL
... type APC modular batteries , and/ ... the SE modular batteries such as GVSBTU ... ... 100kva and the PX 250/500kva UPS units) batteries . Note – SYBTU1-PLP and SYBTU2-PLP use batteries manufactured by four different vendors. ... Galaxy VS Modular Batteries : Battery Type ... 1 .057 ... Battery Type ... 1 ... Battery Type
Electrolyte Levels of All Single-phase Symmetra Battery Systems
SYBATT: Each SYBATT contains (10) 12V 7.2ah batteries installed in series.
APC UPS Network Management Card (NMC) Compatibility Chart
Symmetra PX 250/500 ... Symmetra PX 20/40/80 Symmetra PX2 48kw All-in- One * Symmetra PX2 100/ 160 kW *
Buzzing sound coming from a single phase Symmetra
All manufactured systems in the above product lines ... This can become especially apparent when installing new power modules or comparing the noise between two different Symmetra LX systems. ... The inverters in the power modules will emit a buzz or hum noise during online and on battery operation.
How to Cold Start a Symmetra LX Extended Run Frame
The extended run frame needs to have at least one good battery installed with the black knob on the front of the battery in the ...


Resultados 1 - 10 de 85

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.