Consultar las preguntas frecuentes



APC Schneider Cooling Unit Identification
... -230/ 3 / 60 ... = 480/ 3 / 60 ... = 600/ 3 / 60 E= Electric A= 3 row 20 ... -230/ 3 / 60 ... = 480/ 3 / 60 ... = 600/ 3 / 60 ... /208/ 3 / 60 ... /208/ 3 / 60 ... /480/ 3 / 60 ... /208/ 3 / 60 F= Electric ... = 600/ 3 / 60 ... /208/ 3 / 60 ... /208/ 3 / 60 ... /480/ 3 / 60
What are the operational conditions for an InRoom (Stulz) Unit
... °F) Upper limit : Depending on ... ... / 3ph / 60 Hz ... / 3ph / 60 Hz ... imbalance: < 3 % Frequency: 60 Hz +/ ... Maximum water head pressure ... Maximum equivalent length of ... cooled condenser: 60 m (200 ... Maximum level difference between ... Return air conditions for evaporator capacity ( DX ): 24°C (75°F) 50% R. H. ... Maximum condensing temperature: 60 °C (140°F) Cooling fluid ( DX ): 30% Glycol ... Data is valid for: 460v / 3ph / 60 Hz
Network Air FM unit spare parts list
CKT BKR 3 P 20a 480vac ... CKT BKR 3 P K 16A ... CKT BKR 3 P K 20a ... CKT BRKR 3 P 100a 600v ... CKT BRKR 3 P 150a 600v ... CKT BRKR 3 P 25A 480v ... CKT BRKR 3 P 30a 600v ... CKT BRKR 3 P 40a 480v ... CKT BRKR 3 P 40a 600v ... CKT BRKR 3 P 50a 600v ... CKT BRKR 3 P 60a 480v ... CKT BRKR 3 P 70a 600v ... ... FIX SOLUTION # 3 ... FM 35 KW DX ... FM 40 KW DX ... FM 50 KW DX ... humidifier [K 3 ] & heater ...
How to navigate through an Network Air FM unit display
... APC NetworkAIR FM DX Precision Air Conditioner ... DX ... Direct expansion ( DX ) coil ... —Economizer and DX coils ... water) and DX coils ... the NetworkAIR FM DX 60 Hz Up to three Modules can be ... ... valve which feeds three quarters of the ... ... the NetworkAIR FM DX 60 Hz Installation ... the NetworkAIR FM DX . Max ... —Use the maximum value reported by ... DX ... head pressure in DX Systems). ... valve as a three -way valve ... ... valves are always three -way valves ... ... valve as a three -way valve ...
E3 error message on the Symmetra Extended Run Battery Frame (XR frame)
... Symmetra displays E 3 ; The mainframe ... ... The "E 3 " error message ... ... by unscrewing the top right hand thumbscrew ... 3 ) Reseat the ... back into the top right-hand ... ... status light within 60 seconds the UPS ... At this point the E 3 message should no longer be flashing on the XR Frame and on the PowerView you will see a message indicating "Number of Battery Modules Increase".
Information on Online and On Battery operation of 3:1 Symmetra UPS systems
... Battery operation of 3 :1 Symmetra ... 3 :1 ( ... ... Battery operation of 3 :1 Symmetra ... ... When a Symmetra 3 :1 is ... power from all 3 phases, i ... each of the 3 phases. ... phase with a maximum 16KVA load. The 3 phase power is ... ... square root of 3 ) The Symmetra 3 :1 will ... ... at 50 or 60 Hertz. ... no more than 60 amps per phase ... ... , if all 3 phases fail it ... When Symmetra 3 :1 is ... ... While current is evenly distributed across all three phases while Symmetra 3 : ...
Why is my ACRP excessively cycling?
The ACRP DX needs to be given a constant heat load of at 12kw or more. ... The cool setpoint controls the fan speed based on the maximum rack inlet temperature. ... These 2 setpoints should typically be 3 -7F apart.
EcoBreeze Variable Speed Drive Technical Spec’s
... 240 V- 3 -phase supply ... ... 60 Hz (- ... ... number of phases 3 phases Maximum transient current 99 A for 60 s ... 2, L 3 , U, ... ... braking resistor for 60 s ... 2, L 3 , U, ... ... Analogue input number 3 ... voltage 30 V max , impedance 30000 ... ... voltage 30 V max , impedance 30000 ... Maximum switching current R ... ... function, for three phases supply drive ... -5 level 3 Electrical fast transient ... ... -2 level 3 ... -4- 3 level 3 ... (f = 3 ... ...
Video: How do I properly reset a Symmetra XR Frame Communications Card (SYXRCC or SYAFSU16)?
3 ) Reseat the micro-latch on the card and screw in the thumbscrew back into the top right-hand corner of the card. 4) Reconnect the communication cable(s) in the back of the card and acknowledge the return of the green status light within 60 seconds the UPS will re recognize the additional batteries and adjust the runtime value accordingly to include the batteries located in the Extended Run Frame.
Uniflair Humidifier Water Quality
Maximum ... ) 100 Temporary hardness mg/l 60 ( 3 ... ( 3


Resultados 1 - 10 de 75

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.