Consultar las preguntas frecuentes



Network Air FM unit spare parts list
... 25 Pin Cable Lower (Downflow) ... 25 Pin Cable Lower (Upflow) CKT BKR 3 P 20a 480vac ... CKT BKR 3 P K 16A ... CKT BKR 3 P K 20a ... CKT BRKR 3 P 100a 600v ... CKT BRKR 3 P 150a 600v ... CKT BRKR 3 P 25A 480v ... CKT BRKR 3 P 30a 600v ... CKT BRKR 3 P 40a 480v ... CKT BRKR 3 P 40a 600v ... CKT BRKR 3 P 50a 600v ... CKT BRKR 3 P 60a 480v ... CKT BRKR 3 P 70a 600v ... ... FIX SOLUTION # 3 ... FM 35 KW DX ... FM 40 KW DX
APC Schneider Cooling Unit Identification
... -230/ 3 / 60 ... = 480/ 3 / 60 ... = 600/ 3 / 60 E= Electric A= 3 row 20 ... -230/ 3 / 60 ... = 480/ 3 / 60 ... = 600/ 3 / 60 ... /208/ 3 / 60 ... /208/ 3 / 60 ... /480/ 3 / 60 ... /208/ 3 / 60 F= Electric ... = 600/ 3 / 60 ... /208/ 3 / 60 ... /208/ 3 / 60 ... /480/ 3 / 60
What are the operational conditions for an InRoom (Stulz) Unit
... ambient conditions: Lower limit : -10 ... ... / 3ph / 60 Hz ... / 3ph / 60 Hz Voltage imbalance: < 3 % Frequency: 60 Hz +/- 1% ... Maximum equivalent length of piping between the cooling unit and the air cooled condenser: 60 m (200 ft) ... Return air conditions for evaporator capacity ( DX ): 24°C (75°F) 50% R. H. ... Maximum condensing temperature: 60 °C (140°F) Cooling fluid ( DX ): 30% Glycol ... Data is valid for: 460v / 3ph / 60 Hz
ACRP1XX, ACRD5XX, ACRP5XX, and ACRC5XX Parts List
... 0989 ADPTR PIPE 3 " ENGL TO ... ... , GAS SHUTOFF 3 /4" ... ... - acrp1xx ( DX ... (CW AND DX ... FAN acrp1xx ( DX ) ... Reheat acrp1xx ( DX ) ... for acrp1xx ( DX ) ... /102 ( DX ) ... For acrp101 ( DX ) ... for acrp100 ( DX ) ... for acrp101 ( DX ) VAC 3 Phase - Spare ... VAC 3 Phase - Spare ... ... r0357 Circuit Breaker 3 P 10a 280v ... r0457 Circuit Breaker 3 P 10a 480v ... r0427 Circuit Breaker 3 P 15A 480v ... r0457 Circuit Breaker 3 P 20a 240v
How to navigate through an Network Air FM unit display
... APC NetworkAIR FM DX Precision Air Conditioner ... DX ... Direct expansion ( DX ) coil ... —Economizer and DX coils ... water) and DX coils ... the NetworkAIR FM DX 60 Hz Up to three Modules can be ... ... valve which feeds three quarters of the ... Comp Min ON. ... Reducing the Comp Min ON Comp Min OFF. ... Reducing the Comp Min OFF ... the NetworkAIR FM DX 60 Hz Installation ... the NetworkAIR FM DX . DX ... head pressure in DX Systems). ... valve as a three -way valve ... ... valves are always three -way valves ...
Why is my ACRP excessively cycling?
The ACRP DX needs to be given a constant heat load of at 12kw or more. ... These 2 setpoints should typically be 3 -7F apart. In low load situations, the optimal setpoints often differ based on the specific room configuration.
How to read a pressure temperature chart for super-heat and sub-cooling calculations
All DX Cooling units. ... often used for three purposes: to ... Some of the zeotropic blends have very low glide (from I° F to 2.5° F). ... For a single-component or azeotropic refrigerant, the operating pressure for the low side of a system can be found by cross referencing the desired coil temperature on the PT chart. ... In this case, you must add half of the temperature glide to the desired midpoint temperature, then read the saturated vapor column to determine the operating pressure (see Figure 3 )
PowerChute Network Shutdown reports "Available runtime has been exceeded".
For conditions 3 and 4 below ... ... duration and a 60 second OS shutdown ... Condition 3 for VMware: ... greater than the Low Battery Duration minus ... ... event of a low battery condition, ... ... time required is 3 minutes and Low Battery Duration is ... ... duration and a 60 second OS shutdown ... ... greater than the Low Battery Duration minus ... ... event of a low battery condition, ... ... time required is 3 minutes and Low Battery Duration is ... Increase the Low Battery Duration value ... Condition 3 for VMware: Increase the Low Battery Duration value ... Increase the Low Battery Duration value on the NMC using Configure - Shutdown or decrease the shutdown durations being used by PowerChute.
Uniflair Humidifier Water Quality
Minimum ... ) 100 Temporary hardness mg/l 60 ( 3 ... ) Not lower than 200% of the Chloride content in mg/l di Cl- ( 3 ) Not lower than 300% of the Chloride content in mg/l di Cl-
Smart-UPS fan operation parameters
3 . The UPS has a load greater than 75%. 4. The internal temperature of the UPS has reached greater than 140 degrees F ( 60 degrees C). Note, for 4th Generation units (model number begins with SUA ... On these units the fan will always be on in low speed mode, and will switch to high speed mode should one of the following events occur: ... 3 . The UPS has a load greater than 75%.


Resultados 1 - 10 de 76

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.