EcoBreeze Variable Speed Drive Technical Spec’s
... 28.5 kVA ... ... 30 V ≤ 100 ... ... , input voltage 30 V max , ... input voltage 30 V max , ... ... 5 A at 30 V DC, ... R1-R2 on inductive load, 2 A at 250 V AC, cos phi = 0.4, L/R = 7 ms R1-R2 on inductive load, 2 A at 30 V DC, cos phi = 0.4, L/R = 7 ms