Consultar las preguntas frecuentes



Data Center Expert | How do hardware and software support contracts work?
... hardware warranty and software support contracts work for StruxureWare Data Center Expert . StruxureWare Data Center Expert (DCE) - Basic Appliance (AP9465 ... StruxureWare Central (SWC ... StruxureWare Data Center Expert (all versions ... StruxureWare Central (all ... Software Support Contract StruxureWare Data Center Expert appliances come with ... software support. The Data Center Expert appliance and any ... active and complete software support in order to receive technical support and software upgrades. Software support contracts are required for ... covered under base software support SKUs) ... ... currently require support contracts . Hardware Support Contracts
Why does StruxureWare Data Center Expert not accept my One Time passcode?
StruxureWare Data Center Expert is not accepting ... StruxureWare Data Center Expert StruxureWare Central / Data Center Expert all versions. SturuxureWare Data Center Expert requires a 64 ... and the Data Center Expert's MAC address. 1 . In a ... AP9465 = StruxureWare Data Center Expert Basic ap9470 = StruxureWare Data Center Expert Standard AP9475 = StruxureWare Data Center Expert Enterprise AP94VMACT = StruxureWare Data Center Expert Virtual Machine SFDCOBASE = StruxureWare Data Center Operation ... VM or Data Center Operation. ... a word processing application such as notepad ... 11. Launch your Expert client. ... 14. Paste the license key(s) one at a time into the popup box.
StruxureWare Data Center Expert v7.4.2 is no longer available
Resolution If you are using Data Center Expert v7.3.1 or earlier and want to update your software to address the password storage vulnerability, you can update to v7.4.1. You must have a valid support contract to receive the software update. To update from versions earlier than v7.3.1, contact your local Technical Support .
How can I resolve “Failed to create java virtual machine.” error when launching StruxureWare Data Center Expert client?
... Upon launching the StruxureWare Data Center Expert client an error ... StruxureWare Data Center Expert StruxureWare Client potentially any ... StruxureWare may be attempting ... 1 ) Navigate to the Installation directory for StruxureWare Data Center Expert . (default directory is: C:\ Program Files (x86)\ StruxureWare Data Center Expert X.X.X) ... -vm "C:\ Program Files (x86)\ StruxureWare Data Center Expert 7.2.7\dcexpert\jre\bin\javaw.exe" ... 6 )If the issue still persists, please contact your local technical support .
Data Center Expert | How do I upgrade my appliance version?
Process for upgrading StruxureWare Data Center Expert . ... StruxureWare Data Center Expert (DCE) - Basic Appliance (AP9465) ... StruxureWare Data Center Expert (all versions) ... You must have a valid currently active software support contract to recieve upgrade files. ... For other customers worldwide, please contact your local technical support to receive upgrade files. 1 ) Extract the downloaded upgrade zip file.
Where can I find information on the newest release of StruxureWare Data Center Expert?
To obtain the link to download the software , you must contact technical support at this time.
Can I transfer license keys between StruxureWare Data Center Expert servers?
Tech support will look to validate support contracts in order to do this transfer.
Why isn't my DNS change saving in StruxureWare Data Center Expert?
Changing DNS entries in StruxureWare Data Center Expert UI for VM does not save changes. ... StruxureWare Data Center Expert ... StruxureWare Data Center Expert VM with single NIC configured ... It has been seen where changing a DNS entry in StruxureWare Data Center Expert (DCE) when using the console application does not cause the system to reboot and save the DNS changes. This only happens on a system with a single NIC so it is not seen on the DCE hardware servers, only on a DCE VM server.
Restoring StruxureWare Data Center Expert backup to a new Virtual Machine causes system to not fully boot up.
Restoring StruxureWare Data Center Expert backup to a ... StruxureWare Data Center Expert StruxureWare Data Center Expert Virtual Machine ( ... Migrating a StruxureWare Data Center Expert hardware server to ... ... equivalents for the StruxureWare Data Center Expert Basic , Standard, ... An error will occur on the primary interface, and the StruxureWare Data Center Expert virtual appliance will not start. 1 . Gracefully shut down the virtual appliance. ... See StruxureWare Data Center Expert virtual server equivalent configurations. ... Changes in the disk space will take effect once the StruxureWare Data Center Expert virtual appliance has restarted.
Starting with a fresh install of StruxureWare Data Center Expert.
How do I start fresh with StruxureWare Data Center Expert ? ... StruxureWare Data Center Expert ... StruxureWare Data Center Expert any version ... There are multiple reasons someone may want to start fresh with a software such as StruxureWare DCE. ... If you do not have the current version, you may need to contact your local tech support to obtain the download link.


Resultados 1 - 10 de 61

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.