Consultar las preguntas frecuentes



Where can I find information for Data Center Operations web services API (Application Programming Interface)?
The StruxureWare Data Center Operation Web Service API is a set of web services that provide ... to various parts of StruxureWare Data Center Operation .
How to properly set FM condenser set points
FM Condenser Set Points a350 Controller ... Data Center Cooling ... The OHEs use a350a/B and s350a/B temperature controllers to regulate fan operation . ... Fan Config . ... a350 Set
Humidity Issues in IT Data Centers
Humidity Issues in IT Data Centers ... Data Center . ... There are three concerns with humidity in a data centers depending on the type of equipment in the data center ... * Tape drive operation - Humidity can dramatically affect a tape drive’s ability to read and write data. ... The default setting for NetBotz Appliances are 20-50% which may be conservative depending on the equipment in the data center .
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
StruxureWare Data Center Expert is not ... StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... SturuxureWare Data Center Expert requires a ... and the Data Center Expert's MAC address ... StruxureWare Data Center Expert (DCE ... ... = StruxureWare Data Center Expert Basic ap9470 = StruxureWare Data Center Expert Standard AP9475 = StruxureWare Data Center Expert Enterprise AP94VMACT = StruxureWare Data Center Expert Virtual Machine SFDCOBASE = StruxureWare Data Center Operation ... D. Serial number is located on the top front of a hardware DCE server and in help and about in a VM or Data Center Operation . ... 12. Select System -> Server Administration Settings -> License Keys
Where can I get support for APC and MGE Products?
Data Center Facility Cooling - Andover Continuum or TAC Vista Data Center Facility Power - PowerLogic ION Enterprise Data Center Software Integration Kits Data Center University ... InfraStruxure for Large Data Centers InfraStruxure for Medium Data Centers ... InfraStruxure for Small Data Centers ... Operations Capacity Operations Change Operations Energy Cost Operations Energy Efficiency Operations Insight Operations Mobile Operations VIZOR ... Power Ready Notebook Cases ... Software Configuration ... StruxureWare Operations Suite
Can you change the cycle time on an InRow ACRD?
Data Center Cooling ... The unit cannot operate in Lead/Lag mode under InRow operations . You will have to select HACS,RACS or Spot allowing you to access operational screen to configure Lead/Lag. ... Runtime balancing can be enabled through the following path: Configure Group->Runtm Bal.
My Micro DC came with clamp-on ferrites. Where do they go, and are there installation instructions?
The Micro Data Center SX International units ship with one snap-on ferrite per piece of installed equipment. ... Ferrite is installed onto the network communications cable to reduce high frequency RF interference, and is required for 50 Hz operation .
Unlicensing a Camera from NetBotz Central Results in Deletion of Associated Surveillance Pictures
StruxureWare Data Center Expert ... Default operation . ... When a camera is unlicensed from NetBotz Central/ StruxureWare Data Center Expert Surveillance, any existing Surveillance pictures associated with this camera is purged from the server's database. To retain the historical Surveillance pictures for a camera without having it posted future Surveillance pictures to the server, set "Post Mode" to 'Disabled' in Modify Camera Surveillance Settings .
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... describes how to install an acdc1010 Hot ... Install , A Rack ... is a complete set of racks, ... ... is a complete set of racks, ... ... when removing/ installing side panels from ... ... nature of data center loads, this ... operation while the PDU ... ... required to correctly install your Rack Expansion ... ... existing system, install two 21 U ... ... page 5 before installing any side panels ... ... you plan to install a Rack Expansion ... ) must be installed on the PDU ... ... enclosures before you install the joining brackets ... enclosures before you install the joining brackets ... enclosures before you install the joining brackets
What are the typical uses for an EcoAisle System
Install ... year-round operation , with the ... ... critical to smooth operation of a data center . ... of a data center can cause thermal ... ... adequate for proper operation . • As blade servers become a more relied upon server platform, new cooling problems arise in the data center . ... In an open aisle / row configuration the cooling system is typically oversized compared to the power consumed by the IT load. ... Typical data center cooling looks at the temperature of the room to adjust capacity. ... ● Data center expansion ... ● Data center retrofits


Resultados 1 - 10 de 73

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.