Consultar las preguntas frecuentes



Guidelines for installation of an acsc100, or acsc101
... to ducting and wiring. Ensure the room is insulated to minimize the influence of exterior heat loads.
Does my Smart-UPS have Equipment Protection Policy (EPP) coverage?
Any unit installed outside of the U.S. or Canada
Galaxy 5000, Galaxy 5500; Dust Covers
MGE Galaxy 5000, Galaxy 5500, Dust Cover, Input Wiring, Installation , foreign conductive particles,
How much exhaust clearance is needed for a NetShelter CX cabinet?
Cox, exhaust, clearance, installation , heat , overheat, overheated,
DAC, Cancoil Installation Manual
... how to properly install a legacy DAC ... Install Installation and Operating Instructions ... , medium and high temperature refrigeration applications. ... equipment, proper installation and set- ... ... cfm (of outside ventilation) per ... Installation Date __ ... Use high temperature silver solder or ... ... that will cause HEAT GAIN, it ... ... properly sized and installed to insure oil ... ... to minimize external heat gain and condensation ... ... risers should be installed with a trap ... ... have additional options installed . ... omponents have been installed . During periods of warm outdoor temperature, the liquid returns to the refrigerant receiver, and the condenser returns to full capacity.
Whether to install a suction line drier or liquid line drier
Installing a suction line drier in an ACRP DX is a tight fit, but possible. The obvious benefit of a suction line filter drier is the added protection given the system if a burnout should occur. The filter will effectively prevent contamination resulting from the failure from traveling back through the suction line into the other parts of the system. This will minimize the contamination remaining in the system when the inoperative compressor is removed. With this said, it is preferred to put the drier in the suction line. If a technician cannot find a suitable suction line drier with replaceable cores to fit inside the ACRP, a liquid line drier would be fine. It is ok to use an additional liquid line drier with replaceable cores. This can be handy since a technician will have more room on the outside liquid line to install isolation valves to keep the downtime to a minimum when replacing cores. The ACRP uses Danfoss liquid line drier pn # 023z4581, 5/8" ODF SOLDER. You will need to find a small suction line filter drier. After the cleaning procedure is completed, recheck in approximately one to two weeks to ensure that the system condition and operation is completely satisfactory.
Is there a depth extender for the rear or front of NetShelter SX cabinets? Is there a way to bay the rear of cabinets that are different depths?
The EcoAisle product line offers depth extenders. They can also be used outside of an EcoAisle installation .
What is the proper method to secure a NetShelter SX to the floor, and what are the bolt patterns?
... mounting bracket and ar7701 Bolt-Down Kit in the illustrations below are installed both inside and outside of the cabinet.
What are your Cooling Product Energy efficiency rating (EER)?
Install ... EER is generally calculated using a 95F outside temp and an inside (actually return air) temp of 80f and 50% relative humidity. ... = rated heating capacity output (kW)/ heating input power (kW)
What are the typical uses for an EcoAisle System
Install ... the aisles with heat removed directly from ... The deployment of the Active Flow Controller more closely couples the cooling equipment to the IT heat load as it monitors the pressure inside vs outside the containment allowing the fan speed to be adjusted so that the right amount of air is being provided. ... The Active Flow controller looks at the pressure inside vs outside the aisle allowing it to quickly detect the dynamic load changes and send a control signal to adjust the airflow of the cooling equipment.


Resultados 1 - 10 de 99

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.