Consultar las preguntas frecuentes



Hardwiring to 120v, 208v, and 240v loads from a 208v/240v SmartUPS RT UPS
... creates a traditional 240 v/ 120 v panel where there are 2 legs of 120 v and from hot ... would measure 240 volts .
How do I update the firmware of my SMT, SMX, SMC, SRT, XP, or XU series Smart-UPS?
Devices that do *NOT* have upgradable firmware: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.
Video: How do I update the firmware of my SMT, SMX, SMC, or SCL series Smart-UPS using the Firmware Upgrade Wizard?
Issue: There are two methods to update the firmware of the UPS: units are 120 V devices built prior to date code 1037)
Video: How do I configure a 208v Smart-UPS RT or SRT for use with a 240v input?
If you need 120 v for your equipment you will still need to use a stepdown transformer.
What are the basic troubleshooting steps for the Smart-UPS smx1500rm2u ?
... connected to utility power . ... sure that the power cable is securely ... to the utility power supply. ... no input utility voltage ... Check the utility power supply to the ... ... check the utility voltage . ... connected to utility power There is very high, very low, or distorted input line voltage . ... Test the input voltage with the utility voltage display. ... The UPS will restart automatically when utility power is restored. ... Contact APC Support for further assistance. ... The UPS will return to normal operation when the power is restored and the battery has a sufficient charge. ... (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smx750 / smx1000 / smx1500 ?
... connected to utility power . ... sure that the power cable is securely ... to the utility power supply. ... no input utility voltage ... Check the utility power supply to the ... ... check the utility voltage . ... connected to utility power There is very high, very low, or distorted input line voltage . ... Test the input voltage with the utility voltage display. ... The UPS will restart automatically when utility power is restored. ... Contact APC Support for further assistance. ... The UPS will return to normal operation when the power is restored and the battery has a sufficient charge. ... (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smt750 / smt1000 / smt1500 ?
... connected to utility power . ... sure that the power cable is securely ... to the utility power supply. ... no input utility voltage ... Check the utility power supply to the ... ... check the utility voltage . ... connected to utility power There is very high, very low, or distorted input line voltage . ... Test the input voltage with the utility voltage display. ... The UPS will restart automatically when utility power is restored. ... Contact APC Support for further assistance. ... The UPS will return to normal operation when the power is restored and the battery has a sufficient charge. ... (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smt3000rm2u / smt3000 / smt2000rm2u / smt2000 ?
... connected to utility power . ... sure that the power cable is securely ... to the utility power supply. ... no input utility voltage ... Check the utility power supply to the ... ... check the utility voltage . ... connected to utility power There is very high, very low, or distorted input line voltage . ... Test the input voltage with the utility voltage display. ... The UPS will restart automatically when utility power is restored. ... Contact APC Support for further assistance. ... The UPS will return to normal operation when the power is restored and the battery has a sufficient charge. ... (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smx2000hv / smx3000hv ?
... connected to utility power . ... sure that the power cable is securely ... to the utility power supply. ... no input utility voltage Check the utility power supply to the ... ... check the utility voltage . ... connected to utility power The input circuit ... ... distorted input line voltage . Test the input voltage with the utility voltage display. ... The UPS will restart automatically when utility power is restored. Fault LED illuminates Possible Internal Fault Contact APC Support for further assistance. ... The UPS will return to normal operation when the power is restored and the battery has a sufficient charge. ... (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smx2000lv / smx3000lv ?
... connected to utility power . ... sure that the power cable is securely ... to the utility power supply. ... no input utility voltage Check the utility power supply to the ... ... check the utility voltage . ... connected to utility power The input circuit ... ... distorted input line voltage . Test the input voltage with the utility voltage display. ... The UPS will restart automatically when utility power is restored. Fault LED illuminates Possible Internal Fault Contact APC Support for further assistance. ... The UPS will return to normal operation when the power is restored and the battery has a sufficient charge. ... (Applicable for 120 V units only.)


Resultados 1 - 10 de 64

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.