Consultar las preguntas frecuentes



How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
The instructions to power down the UPS are available on the display. This procedure is for a single UPS with an external maintenance bypass panel.
Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
2.) Utilize an APC ap9600 single slot SmartSlot expansion chassis and extend the cable to the ap9600 with a 940- 1500 serial ...
How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX?
... do I connect a EPO (Emergency ... ) circuit to Galaxy VX ? Galaxy VX ... do I connect a EPO (Emergency ... ) circuit to Galaxy VX ? ... A35JB8_R 1 _EN. ... When the UPS is EPO'd, ... ... option in the UPS Tuner ( ... to have the UPS go to static ... ... The UIB ( Unit Input Breaker) ... Tripping of the upstream breaker could be a code requirement, typically if UPS is located in the data center. ... Note; in parallel systems, only the UPS in which the EPO is activated is affected; remaining UPS will still be powered.
Video: How to take Galaxy VM UPS out of Maintenance Bypass
... How to take Galaxy VM UPS out of Maintenance Bypass Galaxy VM ... equipment, the UPS must be transitioned ... -line from maintenance bypass following service or other maintenance to the system ... ... the UIB ( Unit Input Breaker) ... , takes about 1 -2 minutes ... ... Select Startup from Maintenance Bypass ... the MBB ( Maintenance Bypass Breaker) ... top of the UPS and turn the key so the UPS can now go ... ... This video provides a step by step ... to operate the Galaxy VM UPS from Maintenance Bypass mode to ... back to the UPS from MBP without ... Also to transition UPS into Maintenance Bypass
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
... Down the MGE Galaxy 5000 UPS Galaxy 5000, Galaxy 5500 ... Due to site maintenance , inclement weather ... Powering Down the Galaxy 5000 UPS ... power down the UPS are available on ... ... procedure is for a single UPS without an external ... Step 1 : Touch any ... ... Scroll to “ Maintenance ... “Stop the UPS ... protected by the UPS . ... : Turn the maintenance bypass switch Q3BP ... The UPS is now fully isolated from the load. ... Step 6: Turn the Q 1 Switch to Off ... There is still stored energy in the capacitors, and batteries inside the UPS . Never remove any covers or panels.
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from total power ... Galaxy 5000, Galaxy 5500 ... reasons, the Galaxy 5000 may be in a totally off state ... ... not for commissioning a new UPS . ... The commissioning of a new UPS must be performed by a Schneider Electric trained ... ... to restore the Galaxy 5000 UPS from total power ... ... procedure is for a single UPS without an external ... Step 1 : Set the input Q 1 switch to On ... end of the UPS initialization with PFC ... ... Scroll to “ Maintenance ... “Start the UPS ... : Turn the maintenance bypass switch Q3BP ...
Serial communications between Smart-UPS VTs, Galaxy 3500, and Symmetra PX with IBM AS/400, i Series
... configure Smart- UPS VTs, Galaxy 3500, and ... ... 3-phase UPS systems. ... customer already has a AP98275 cable kit ... they would to a Symmetra LX as ... ... port unless in Maintenance Bypass, as there is always a risk of load ... ... *remember that a Field Engineer could ... dispatched to set a UPS to ‘never ... ... is to run a script on some ... *Available UPS Signalling Options for ... ... this by replacing a ap9607 with a ... 3-phase UPS )
​How to read Modbus Status bits
Below is a couple of examples from a Galaxy VX : Example 1: Register 400002 (16385)
Modbus; How to read Status bits
Below is a couple of examples from a Galaxy VX : Example 1: Register 400002 (16385)


Resultados 1 - 10 de 64

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.