Consultar las preguntas frecuentes



How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
... to take the Single Galaxy 5000 UPS from normal operation ... using an external Maintenance Bypass Panel. Galaxy 5000 , Galaxy 5500 ... Due to site maintenance , inclement weather ... Powering Down the Galaxy 5000 UPS ... power down the UPS are available on ... ... procedure is for a single UPS with an external maintenance bypass panel. Step 1 : Touch any ... ... Scroll to “ Maintenance ... “Stop the UPS ... protected by the UPS . ... the MBP ( Maintenance Bypass Panel) ... The UPS is now fully ... ... : Open the UPS door. ... Turn off Q 1 Switch
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
... Down the MGE Galaxy 5000 UPS Galaxy 5000 , Galaxy 5500 ... Due to site maintenance , inclement weather ... Powering Down the Galaxy 5000 UPS ... power down the UPS are available on ... ... procedure is for a single UPS without an external ... Step 1 : Touch any ... ... Scroll to “ Maintenance ... “Stop the UPS ... protected by the UPS . ... : Turn the maintenance bypass switch Q3BP ... The UPS is now fully isolated from the load. ... Step 6: Turn the Q 1 Switch to Off ... There is still stored energy in the capacitors, and batteries inside the UPS . Never remove any covers or panels.
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from total power ... Galaxy 5000 , Galaxy 5500 ... reasons, the Galaxy 5000 may be in a totally off state ... ... not for commissioning a new UPS . ... The commissioning of a new UPS must be performed by a Schneider Electric trained ... ... to restore the Galaxy 5000 UPS from total power ... ... procedure is for a single UPS without an external ... Step 1 : Set the input Q 1 switch to On ... end of the UPS initialization with PFC ... ... Scroll to “ Maintenance ... “Start the UPS ... : Turn the maintenance bypass switch Q3BP ...
Information for Colors of UPS Galaxy 5000, Galaxy 5500
Product line: Galaxy 5000 , Galaxy 5500
​Information for Noise level of UPS Galaxy 5000 NAM
UPS rating ( kVA ) 40/ ... Noise level on a normal floor (dBA) with an RL load at 3 feet 65 63
Video: How to take Galaxy VM UPS out of Maintenance Bypass
... How to take Galaxy VM UPS out of Maintenance Bypass Galaxy VM ... equipment, the UPS must be transitioned ... -line from maintenance bypass following service or other maintenance to the system ... ... the UIB ( Unit Input Breaker) ... , takes about 1 -2 minutes ... ... Select Startup from Maintenance Bypass ... the MBB ( Maintenance Bypass Breaker) ... top of the UPS and turn the key so the UPS can now go ... ... This video provides a step by step ... to operate the Galaxy VM UPS from Maintenance Bypass mode to ... back to the UPS from MBP without ... Also to transition UPS into Maintenance Bypass
What are the shipping dimensions of the Galaxy 5000 UPS
Galaxy 5000 shipping dimensions ... Galaxy 5000 ... Aids customer in knowing if the UPS on a pallet or its own height on casters will clear the doors when moving to install location. ... UPS : 1 @ 37.8X38.58X79.92" H + 1 @ 33x30x76" H + 1 @ 16x14x7" H (2,902.26 lbs, 2 spots due to dimensions) Batt. Cab: 1 @ 40x40x75" H (2,835 lbs, 2 spots due to dimensions)
Galaxy 5000, Galaxy 5500; Dust Covers
It has been determined that dust and other foreign conductive particles have been getting inside the UPS during shipping or from site construction projects during installation. ... Galaxy 5000 , Galaxy 5500 ... Temporary front and top covers are being applied to Galaxy 5000 units prior to shipping to protect the unit from foreign particles. ... Only Schneider Electric Certified Field Service Engineers are authorized to remove this cover.
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... , N and 1 . Slave address is 1 and wiring is ... ... This assumes only one 66061 card or UPS or STS is ... ... Monitoring Enclosure has a CB, power ... One is down ( ... ... Modbus card has a female DB9 so a male DB9 cable ... required on the UPS /STS. The male DB9 connector is not supplied with the UPS but a black terminal block is supplied with the EGX.
Serial communications between Smart-UPS VTs, Galaxy 3500, and Symmetra PX with IBM AS/400, i Series
... configure Smart- UPS VTs, Galaxy 3500, and ... ... 3-phase UPS systems. ... customer already has a AP98275 cable kit ... they would to a Symmetra LX as ... ... port unless in Maintenance Bypass, as there is always a risk of load ... ... *remember that a Field Engineer could ... dispatched to set a UPS to ‘never ... ... is to run a script on some ... *Available UPS Signalling Options for ... ... this by replacing a ap9607 with a ... 3-phase UPS )


Resultados 1 - 10 de 61

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.