Consultar las preguntas frecuentes



Where do I find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC modular batteries
... 80 and 96KVA UPS units as well as the SUVT and Galaxy 3500 UPS units ) and the ... 250/500kva UPS units ) batteries.
What type of battery could I use with the Galaxy VS UPS?
Galaxy VS, 3 Phase UPS , Uninterrupted Power Supply, 10 kVA , 15 kVA ,20 kVA , 20 kVA ,30 kVA ,40kva, ... use with the Galaxy VS UPS ?, battery ...
Video: How can the Galaxy VS reduce my energy bill?
Galaxy VS, 3 Phase UPS , Uninterrupted Power Supply, 10 kVA , 15 kVA ,20 kVA , 20 kVA ,30 kVA ,40kva, ...
What UPS units are officially supported by the ap9610 (Relay I/O SmartSlot Card)?
SURTA SUVT / Galaxy 3500 (Must use Configuration #2 - same as Symmetra)
What UPS units are officially supported by the AP9613 (Dry Contact I/O SmartSlot Card)?
SURTD SUVT / Galaxy 3500 (Must use Configuration #2 - same as Symmetra)
How do I connect a EPO circuit to Smart-UPS VT or Galaxy 3500 Battery XR Frame?
Galaxy 3500 , SUVT , EPO, REPO, g3500, Battery frame, XR frame, XR frame EPO circuit wiring, Installation – ...
Galaxy 3500, Smart-UPS VT and ais3000 Power Factor Information
Galaxy 3500 , Smart- UPS VT and ais3000 Power Factor Information ... Galaxy 3500 , Smart- UPS VT and ais3000 ... Galaxy 3500 , Smart- UPS VT and ais3000 Power Factor Information ... "The SUVT and the ais3000 have an Input Power Factor Correction Module which corrects the Power Factor on the input of the unit . The Input Power Factor is 1 . The Output Power Factor is 0.8 - what means that, for example, a 10kva unit can provide a maximum total load of 8KW. This means there is a difference of 20% between real and apparent power.
Smart-UPS VT-g3500; Load does not turn on automatically after an outage/shutdown
Suvt autostart, Galaxy 3500 Autostart, SUVT turn load on, set auto start to on, restart, how to set auto start ...


Resultados 1 - 10 de 53

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.