Consultar las preguntas frecuentes



Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
... 8 and 10 KVA FAQ ... 5-10 KVA UXI Models turn ... ... equally but if one fails (either ... taken out of service for maintenance ), the ... Q: What are the advantages of the SRC 5-10 KVA LCD Display? ... Q: When do I need to choose a Service Bypass Panel? ... A: In addition to the 1 + 1 Parallel redundancy system, the Customer can also look into a service bypass panel which will give you a wrap around bypass. ... Q: What are the advantages of the aptf10kw01 Isolation Transformer?
3 Phase Products Service Level Agreements; Definition of coverage as relates to the service level agreements offered by SE
Service Level Agreements APC ... ... relates to the service level agreements offered ... 1 Site Inspection Visit 1 set of air ... ... UPS & PDU Advantage Plus : ... _EN_ Advantage Plus 1 Annual PM Visit ... UPS & PDU Advantage Prime: See attached file; ARUO-ACQGSD_R7_EN_ Advantage Prime ... 1 Annual Preventive Maintenance Visit ... UPS & PDU Advantage Ultra: See attached file; ARUO-ACQFVH_R6_EN_ Advantage Ultra ... 1 Annual Preventive Maintenance Visit 1 Set of air filters if applicable ... TSE agent will follow internal protocol to handle the service coverage and necessary actions to process customer requests per SLA.
Where can I get support for APC and MGE Products?
Assessment Services ... Battery Replacement Services ... Environmental Monitoring Unit ... Installation Services ... Maintenance Bypass Panels ... MGE Service Bypass ... Network Integration Services ... On Site Service ... Planning Tools and Publications ... Power Distribution Units ... PowerChute plus ... Preventive Maintenance Project Management Services ... Remote Monitoring Services ... Service Bypass Panel Service Plans ... Start-Up Service Stationary Power Distribution Units ... Symmetra MW Symmetra MW Accessories ... Training Services
What are the Dynamic Load ratings and Shipping Load ratings for NetShelter CX cabinets?
Persons planning data centers need ... ... the cabinet, plus installed equipment ( ... These two ratings are different and care should be taken to distinguish between them. ... This is the maximum allowable weight of equipment installed in the cabinet during movement from one location to another within the same data center. ... Example: a customer who wishes to move a cabinet from one row to another in a data center must remove equipment until the weight is equal to (or below) the Dynamic Load Rating before being moved.
How To: Configuring an APC Network Management Card with popular email services such as Gmail, Yahoo!, Office 365, and Hotmail/Outlook.com
Devices with an embedded Web/SNMP Card include (but are not limited to): Environmental Monitoring Unit 1 (AP9312TH)
Video: How to Reset the Service Interval timer on an APC ATS
Select ‘Reset Service Record’ Then select ‘Yes’ to confirm. The date will change to one year in the future.
What do I gain with a Unity Output Power Factor (kW=kVA)?
... (kW= kVA )? ... (kW= kVA )? The advantage of unity power ... Some APC 3-phase UPS products as well as newer single phase products(SRT6K) have an output rating of kW= kVA or Unity Power Factor. While the more traditional double conversion units have output ratings of kW=0.8kva. ... https://www.apc.com/salestools/SADE-5TNQYL/SADE-5TNQYL_R 1 _EN.pdf
Bypass operation of Symmetra Power Array 3:1 (3-Phase Input / 1-Phase Output)
... my 3: 1 Symmetra UPS operate ... 3: 1 (International) ... ... a 3: 1 Symmetra UPS system ... Maintenance Bypass ... by switching the Maintenance Bypass Switch on ... ... Symmetra 3: 1 in bypass 1 . With the ... 1 . Without the ... ... Symmetra 3: 1 will draw all the current from one dedicated phase. ... loads above 12 KVA . ... loads below 12 KVA you can use ... ... breaker on phase one . The Bypass transformer will draw current from 2 (L 1 & L2) of the 3 phases, but no more than 60 Amps per phase.
Why choose glycol over water?
All cooling units that require heat exchangers ... Advantages of Glycol: ... The elimination of corrosion greatly reduces maintenance costs. ... This eliminates the costs of filter maintenance and filtration pump power. ... - Did you know that just 1 /16" of scale reduces heat transfer by 40%!


Resultados 1 - 10 de 85

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.