• Default Alternative Text

    DRaaS, data backup and recovery

    Eliminate data loss, downtime and defend against ransomware. DRaaS provides a comprehensive solution; protecting your critical application, file, folder and cloud data (O365/Google/SFDC) all managed by a single web-based UI.

    Contact Us

Comprehensive solutions for nearly any IT Environment

APC by Schneider Electric has partnered with Infrascale, to offer secure and affordable data backup and disaster recovery solutions. Protect files, folders, email or complete workloads while detecting and mitigating ransomware.

Secure and affordable solutions that are easy to manage

  • Disaster Recovery as a Service (DRaaS)

    Protect critical data and applications. Restore critical business operations in 15 minutes or less with the push of a button.

  • Cloud Backup

    An enterprise grade solution that protects servers, desktops, laptops, tablets and smartphones all in one solution.

  • Cloud Application Backup

    Protect your hosted applications and data with the same retention and recovery options used your other devices, applications and data.

  • 15-minute failover guarantee

    Industry-leading SLA for failover with an average recovery time of 70 seconds.

  • Protect a wide range of systems

    Protect both physical and virtual environments, Windows, Linux, Unix, WMware and Hyper-V.

  • Affordability

    Using the power and scale of the cloud, we can equip every organization with affordable failover and data protection.

  • Central deployment and management

    Configuration and management can all be performed remotely using an intuitive dashboard.

  • Drag-and-drop orchestration workflow editor

    Specify the order in which systems are recovered, create groups, and time intervals for boots to ensure smooth recovery.

  • DR Testing

    No need to declare a disaster or incur additional costs. Test system dependencies before a real emergency hits

  • Ransomware Mitigation

    Anomaly detection alerts if any of your devices have been infected by ransomware

  • Secure replication to the cloud or secondary appliances

    All communications use AES-256 encryption to avoid unauthorized access during data transfers

Default Alternative Text

Solution briefs and case studies

Learn more about this comprehensive approach to protecting your critical data and ensuring availability. Whether data is from mobile devices, cloud based applications or critical servers you can manage all via a common interface.

Back and Recovery Solutions Brief

DRaaS Solution Brief

Case Studies

Failover and recovery at the push of a button!

Learn why Infrascale was ranked the #1 DRaaS solution provider for low to medium complexity environments by Gartner and recognized as a MQ leader. Tour the Disaster Recovery Dashboard and see DRaaS in action and how it can protect almost any IT environment.

See more at Infrascale.com

Default Alternative Text

Want more information?

Whether you are a partner or end user we welcome the opportunity to help you find the security solution that best fits your business needs. Contact us today to schedule a personalized demo.
Request a Demo