Technical FAQs

Ask a Question

Filter results

    What materials are used in the main structure and acoustic foam lining of the NetShelter CX?
    The NetShelter CX also uses a combination of Medium Density Fibre Board ... (HPL) on its top and MDF on its plinth base .
    Where do PDUs mount in the NetShelter CX?
    For a list of APC 0U PDUs that are compatible with all NetShelter cabinets please see Knowledge Base document FA158651.
    Is there a list of NetShelter CX spare parts and accessories available, with photos?
    cx , side, fan, power supply, hinge, fan ... adapter, cx2, mini, key, keys, psu, plinth
    Are NetShelter SX, SV, CX or VX cabinets NEMA rated?
    The word "enclosure" is to be used to describe NEMA rated products. For more information please see Knowledge Base document FA225841.
    acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
    ... Rack Expansion Bundle Kit next to a ... When joining two NetShelter VX (1070-mm) enclosures: ... When joining two NetShelter VX (1070-mm) enclosures: ... When joining a NetShelter VS (900-mm) to a NetShelter VX (1070-mm) enclosure, use rear joining brackets and trim. ... The ceiling panels are configured in two different widths based on the size of the enclosures they span.. ... 3. Attach the plinth blocks to the enclosures, using four M8 × 25-mm screws
    Can the NetShelter CX be locked?
    Issue: The NetShelter CX needs to be locked
    Where can a NetShelter CX be deployed?
    Issue: Where can the NetShelter CX be deployed?
    NetShelter CX Air Filters are Difficult to Install.
    Issue: NetShelter CX Air Filters are Difficult to Install.
    Is the NetShelter CX available in different colors?
    Issue: Customers need to know what colors the NetShelter CX are available in.
    Results 1 - 10 of 50