Browse FAQs



Did APC purchase the AirFlow Company?
Did APC purchase the AirFlow ... APC purchased Airflow in ... Air Division under APC . ... our technical support line to identify the ... Our Tech line will also be ... American Power Conversion Expands Availability Solutions with Acquisition of Airflow Company ... will operate within APC’s Availability Enhancements Group, further strengthens APC’s stature as a ... one-stop shop of availability solutions ... ... the limit, two of the biggest ... ... Jr., APC’s president and CEO ... ... The marriage of APC and Airflow is ... win, providing APC with entry into ... business while leveraging APC’s global scale, ... ... to industry and APC estimates, Airflow ... ... Research Corporation, eight percent of all ...
Cable Picture Degradation When Using an APC Coaxial Surge Protector
After connecting an APC device with Coax Protection , customer observes picture degradation or loss of digital channels. ... SurgeArrest , Protectnet, Back-UPS, Back-UPS Pro, APC AV line of products ... connected which requires 4 dB, the chances of 'ghosting' or lines being present ... Inserting a cable protector like an APC ... APC Coax protection has been tested from 30 MHz to 1 GHz. ... terminated cables from an electronics store ; such as Radio Shack. 2 . Use a 50 ohm terminator for any exposed non-connected female connectors (available at many electronics stores ).
SurgeArrest - minimum install distance of 10 meters (30ft).
... between the electrical outlet and the electrical ... APC Surge Arrest products ... transformer and the line side of the ... Type 2 ... utilization equipment being protected . ... Type 1, 2 , 3 Component ... ... external short circuit protection . ... to the voltage protection rating ... 1 and Type 2 rated surge protection ... UL96A "Lightning Protection Systems" specifications ... A Type 3 surge protection device is not intended for direct lightning protection , therefore it is tested beyond the potentially effected area. ... Ideally for residential use, Type 2 which is often referred to as "TVSS" protection should always be installed at the main electrical service entrance.
Scripting with APC by Schneider Electric Switched Rack Power Distribution Units (PDUs)
... scripting or automating outlet control on Switched ... ... like to automate outlet control actions using ... APC by Schneider Electric ... offer a command line interface for easy scripting to automate outlet control. ... User Name : apc Password : apc ... you're typing for security purposes ... the PDU command line interface: Outlets : 8 ... : ON : Outlet 1 2 : ON : Outlet 2 ... : ON : Outlet 3 ... : ON : Outlet 4 ... : ON : Outlet 5 ... : ON : Outlet 6 ... : ON : Outlet 7 8 : ON : Outlet 8 APC >
How do I configure my RADIUS server to authenticate my APC Network Enabled device?
... set up with APC Network Management Card ... ... Network Management Card 2 (NMC2) ... ... Network Management Card 2 include (but ... to): 2 G Metered/ ... ... Firmware versions v 2 .X. ... ... through testing, APC by Schneider Electric ... 2 ) dictionary shortname = apc 2 ) dictionary VENDOR APC 318 ... BEGIN-VENDOR APC ATTRIBUTE APC -Service-Type 1 integer APC VALUE APC -Service- ... VALUE APC -Service-Type Device 2 VALUE APC -Service- ... # APC local radius authentication ... APC -Service- ...
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... Network Management Card 2 - ap9630/ ... ... Network Management Card 2 include (but ... to): 2 G Metered/ ... ... Network Management Card 2 device from v ... ... Network Management Card 2 ... Network Management Card 2 but MUST APC Technical Support APC offers several different ... ... /www. apc .com/ shop /us/ ... ... /AP9617/ 8 /9 installed ... Network Management Card 2 units with the ... ... Network Management Card 2 device from v ... ... Network Management Card 2 devices (Currently ... and Rack PDU 2 G) ... Card 1 and 2 ... Card 1 and 2
How do I update/change the language pack on my Network Management Card 2 device?
... Network Management Card 2 device? ... Network Management Card 2 - ap9630/ ... ... Network Management Card 2 include (but ... to): 2 G Metered/ ... ... of AOS ( APC Operating System) ... Network Management Card 2 devices (ap9630 ... ap9630), APC now supports localization ... ... Network Management Card 2 in the form ... ... for download via apc .com via ... ... translate the Command Line Interface (CLI ... ... Network Management Card 2's language pack, ... ... Network Management Card 2 Firmware Upgrade Utility ... FTP)/ Secure CoPy (SCP ... ... Network Management Card 2 Firmware Upgrade Utility
Why is my equipment dropped or rebooted while connected to my Smart-UPS?
... be good for 2 years if operated ... 2 ) ... plugged into different outlets that are being ... ... through non- APC serial cable will ... ... cable provided by APC with your UPS or an optional APC cable for your ... All APC serial cables are ... shelf non- APC cable will work ... ... Smart-UPS line interactive units you can expect a 2 -4ms transfer ... ... SURT"" line . 8 ) Controllable Outlets ... configure groups of outlets to turn off ... ... ensure that the outlet group the load ... Each UPS must have its' own pair of wires running back to the EPO switch.
Video: How can I download Event, Data, Configuration, and Debug files from my Network Management Card?
... Network Management Card 2 (NMC2) ... ... Network Management Card 2 include (but ... to): 2 G Metered/ ... ... via the Command Line Interface (CLI ... ... Network Management Card 2 (ap9630, ... 2 .) Change ... want the files stored in. ... in most command line tools. 8 .) ... Network Management Card 2 only, files are now stored in the / ... ... specified in step 2 . ... Network Management Card 2 (ap9630/ ... 2 .) Navigate ... ... Network Management Card 2 (ap9630/ ... " via Command Line Interface
Why is the Protection Working LED of an APC SurgeArrest, or SurgeProtector off?
... Why is the Protection Working LED of an APC SurgeArrest , or SurgeProtector ... APC Surge Arrest ... Reasons the green-colored Working Protection LED of the APC SurgeArrest may not ... 1. The unit is powered off (for 7 outlet SurgeArrest strips only). 2 . The LED is defective. ... If one of the items numbered 2 through 4 is the reason, APC will replace the SurgeArrest under its lifetime warranty. First, check that the SurgeArrest unit's circuit breaker is not tripped. Then check that the SurgeArrest unit is plugged into a good, properly functioning power receptacle outlet .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.