Technical FAQs

Ask a Question

Filter results

Clear
UPDATED: 10-JAN-2018 | Security Notification: "Meltdown" (CVE-2017-5754) and "Spectre" (CVE-2017-5753 & CVE-2017-5715)​ - impact to APC products
Issue Do the "Meltdown" (CVE-2017-5754) and "Spectre" (CVE-2017-5753 & CVE-2017-5715) vulnerabilites impact APC products? Product Line Including but...
Do we have a solution for seismic constraints for the ACSC unit?
Issue: Do we have a solution for seismic constraints?   Product line: ACSC100, ACSC101   Environment: InRow Cooling   Cause:   Resolution: Yes, Use...
What is capacity regulation on an ACRD?
Issue: What is capacity regulation on an ACRD? Product line: ACRD100, ACRD101, ACRD200, ACRD201 Environment: Data Center Cooling Cause: Resolution:...
What are the placement considerations for the fluid cooler relative to the InRow ACRD20x?
Issue: What are the placement considerations for the fluid cooler relative to the InRow ACRD20x? Product line: ACRD200, ACRD201 Environment: Data...
Are the ACSC condenser fans always on? Are they variable speed?
Issue: Are the condenser fans always on? Are they variable speed?    Product line: ACSC100, ACSC101   Environment: InRow Cooling   Cause:   Resolution:...
Does the ACSC automatically restart after a high head pressure alarm?
Issue: Does the ACSC automatically restart after a high head pressure alarm?   Product line: ACSC100, ACSC101   Environment: InRow Cooling   Cause:...
What are the condenser pressure drop and temperature limitations on the ACSC?
Issue: What are the condenser pressure drop and temperature limitations?   Product line: ACSC100, ACSC101   Environment: InRow Cooling   Cause:  ...
How do the evaporator fan speeds work on the ACSC?
Issue: How do the evaporator fan speeds work?   Product line: ACSC100, ACSC101   Environment: InRow Cooling   Cause:   Resolution: There are a few...
How does the ACSC calculate capacity in realtime?
Issue: How does the ACSC calculate capacity in realtime?   Product line: ACSC100, ACSC101   Environment: InRow Cooling   Cause:   Resolution: There...
There is no filter on the condenser side on the ACSC; do I need to clean the coil?
Issue: There is no filter on the condenser side; do I need to clean the coil?   Product line: ACSC100, ACSC101   Environment: InRow Cooling   Cause:...
Results 61 - 70 of 100