Technical FAQs

Ask a Question

Filter results

Clear
AIS3000 External Battery Frame
"The AIS3000 can be attached to External Battery Frames in order to increase the runtime. The maximum number of External Battery Frames is limited...
InRow RC Standard and Optional Features
"1-The Standard Features of the InRow Rc Coolling Unit are as follow: Variable Speed Fans Shutdown Input/Alarm Output Chilled Water Flow Meter 2-way/3-way...
APC InfraStruXure is Coming to a City Near You!
"Come see firsthand how this exciting new architecture can help you easily adapt to the ever changing requirements of your data center or computer...
What is the ACRC Cable Length?
The cable lengths are based on UL electrical standards for that type of device. Per UL the maximum cable length can not exceed 6' and must be at least...
Results 81 - 84 of 84