Technical FAQs

Ask a Question

Filter results

Clear
InRow RC Cooling Units installation distances
"To install an InRow RC unit it is necessary a minimum of 1143mm in front of the unit and 914mm at the back of the unit for maintenance and service...
What rackmount surge protection do you offer?
Issue: What rackmountable surge protection does APC by Schneider Electric offer? Product Line: Protectnet, Surge Arrest Performance, APC AV Power...
What are the battery replacement options for the Smartcell battery pack?
Issue What are the battery replacement options for the Smartcell battery pack? Product Line Matrix UPS Environment Matrix UPS with SMARTCELL battery...
Using D-Link Power Over Ethernet Adapters with NetBotz 320 & 420 Appliances
"High Level Usage Instructions: Mount NetBotz 420 or 320 appliance without needing to have electrical outlet nearby NetBotz 420 or 320 appliance can...
Difference between SYBT5 and SYBT5FR
SYBT5 and SYBT5FR are both the recommended battery modules for Symmetra LX. In dimensions, electrical characteristics, chemical characteristics or...
APC KVM Switches and Corresponding Cables/Server Modules
APC KVM Part Numbers and Corresponding Cables/Server Modules KVMXXXX Series KVM Switches/Cabling The KVMXXXX series of KVM Switches include KVM0108A,...
InfraStruXure Central 4.1.x APC LAN side devices will not communicate after the configuration of the server is backed up and restored.
Issue: InfraStruXure Central 4.1.x APC LAN side devices will not communicate after the configuration of the server is backed up and restored. Product...
This document discusses the maximum number of XR frames allowed with a Symmetra PX solution
"This depends on the size of the Symmetra PX Main Frame. For a Symmetra PX 40kW Frame, the maximum number permitted is 4 fully populated (Battery...
SUVT/AIS3000 Dual Mains
"Yes. The SUVT and the AIS3000 can be used with dual mains connection. One main will go to the normal Input while the another secondary main will...
Halon and FM 200 Leakage and Detection
"NetBotz appliances with the use of third party 4-20mA sensors can be used for detecting leakage of FM-200/Halon. The following third party sensor...
Results 71 - 80 of 84