Technical FAQs

Ask a Question

Filter results

Clear
Supported PCMCIA Modem Cards for WallBotz 500
Issue: Supported PCMCIA Modem Cards for WallBotz 500 Product Line: NetBotz Environment: NetBotz 500 Cause: Supported Accessories Resolution: The part...
USB CAT-5 Pod Extender Specifications
Issue: USB CAT-5 Pod Extender Specifications Product Line: NetBotz Environment: NetBotz CAT5 pod extender Cause: Configuration. Resolution: The NetBotz...
NetBotz Fiber Pod Extender
Issue: NetBotz Fiber Pod Extender Product Line: NetBotz Environment: NetBotz Fiber pod extender. Cause: Product information. Resolution: The NetBotz...
NetBotz Temperature Sensors are NOT Thermocouples
Issue: NetBotz Temperature Sensors are NOT Thermocouples Product Line: NetBotz Environment: All versions Cause: Manufacturing information Resolution:...
NetBotz Central Enterprise Revision D Specifications
Issue: NetBotz Central Enterprise Revision D Specifications Product Line: NetBotz Central Environment: NetBotz Central version 2 revision D Cause:...
NetBotz version 1 and 2 Appliances - MAC Address Ranges
Issue: NetBotz version 1 and 2 Appliances - MAC Address Ranges Product Line: NetBotz Environment: NetBotz version 1 and 2 Cause: Mac address ranges....
Length of the Netbotz Audio-Style Door Sensor
Issue: Length of the Netbotz Audio-Style Door Sensors Product Line: NetBotz Environment: NetBotz version 1 and 2. Cause: Cable length Resolution:...
There are different types of NetBotz Sensor Extender Cables, this article explains what the differences are.
Issue: There are different types of NetBotz Sensor Extender Cables, this article explains what the differences are. Product Line: NetBotz Environment:...
Mounting the Symmetra LX in a 2 post rack
Issue: How do I mount a Symmetra LX in a 2 post rack? Product Line: Symmetra LX Environment: All serial ranges Cause: Symmetra LX ships with a 4 post...
InRow RC Cooling Units installation distances
"To install an InRow RC unit it is necessary a minimum of 1143mm in front of the unit and 914mm at the back of the unit for maintenance and service...
Results 61 - 70 of 87